Sensors
  • Technologies
  • More
Sensors
Sensor Forum Hydroponic system nutrient sensors help
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 21 replies
  • Answers 15 answers
  • Subscribers 361 subscribers
  • Views 7697 views
  • Users 0 members are here
Related

Hydroponic system nutrient sensors help

xan326
xan326 over 13 years ago

Hi all, I'm going to be building a hydroponic system soon being controlled and monitored by a board (most likely beaglebone). But I need help with finding sensors and connecting them, I have literally no idea what connect tivity any boards have (rasberry pi, arduino, beaglebone/beagleboard, atmel) and if they're just USB, then finding a way to convert connections to usb. But I'll get into that later.

The sensors I need are:

Dissolved Oxygen

Hydrogen

Carbon

Nitrogen

Potassium

Phosphorus

Calcium

Magnesium

Sulfur

Boron

Chlorine

Copper

Iron

Molybdenum

Manganese

Zinc

Nickel

Sodium

Cobalt

Selenium

Silicon

Then PH and Flow rate sensors

 

Anyways, if anyone knows of any place to get these sensors please tell me or post a link. Also if they're not natively USB, explain a way (or post a link to an article) on how to convert the connection to usb.

Thanks to everyone that will help! This is my first project using any of the boards like beagle or arduino.

 

Also does anyone know of any pumps; both air and water; that can be run from one of the boards?

  • Sign in to reply
  • Cancel

Top Replies

  • davewr
    davewr over 13 years ago in reply to xan326 +1 suggested
    Just one more note -- if you consider the question answered - mark it as answered as a courtesy to me and to everyone reading the thread. If you have more questions start a new thread with specific questions…
Parents
  • kidiccurus
    0 kidiccurus over 12 years ago

    Seems no one has talked about actually interfacing the sensors with USB so I will try and cover that here. All of the boards you have described can use gpio pins to read sensors, often through i2c. Converting a sensor to usb is not generally desirable unless the final device is a usb connected sensor. Personal recommendation is arduino. It can interface with most things. It can also read analogue values which if often helpful for cheaper sensors. The only reason to use beaglebone or pi is if you want a computer interface or web connectivity, otherwise arduino is cheaper. You also get more gpio per pound (or dollar or euro or yen) with arduino. When you find your sensor I can help you use it correctly.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • kidiccurus
    0 kidiccurus over 12 years ago

    Seems no one has talked about actually interfacing the sensors with USB so I will try and cover that here. All of the boards you have described can use gpio pins to read sensors, often through i2c. Converting a sensor to usb is not generally desirable unless the final device is a usb connected sensor. Personal recommendation is arduino. It can interface with most things. It can also read analogue values which if often helpful for cheaper sensors. The only reason to use beaglebone or pi is if you want a computer interface or web connectivity, otherwise arduino is cheaper. You also get more gpio per pound (or dollar or euro or yen) with arduino. When you find your sensor I can help you use it correctly.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer