Sensors
  • Technologies
  • More
Sensors
Sensor Forum accelerometer or gyroscope
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 10 replies
  • Answers 2 answers
  • Subscribers 350 subscribers
  • Views 1678 views
  • Users 0 members are here
  • accelerometer
  • gyroscope_sensor
Related

accelerometer or gyroscope

e14 Contributor
e14 Contributor over 13 years ago

I'm building a camera stabilizing gimbal for use on a drone helicopter. I would like to smooth out some of the turbulance experienced by the copter in windy conditions. What sensor would better serve my needs, an acclerometer or a gyroscope?  I am only interested in handling values in the X and Y directions. I also notice there are various "g" sensitivities (1.5g, 6g etc.).  Any thoughts on that would help and probably save me time and $$.

Thanks

  • Sign in to reply
  • Cancel
Parents
  • vsluiter
    0 vsluiter over 13 years ago

    Barry,

     

    You'll probably need both; the gyroscope measures angular velocity (degrees/second), which is good for maintaining a constant angle. You just need to integrate the angular velocity to get the angular position, and that way you can keep the camera at a constant angle with respect to your copter.

    However, that's probably not good enough; the gyros have a small error that adds up while integrating (because integrating boils down to adding up samples), and you probably want to keep the angle constant with respect to the earth, not the copter. That's why people use accelerometers. With an accelerometer you can determine the gravitational vector, i.e., you know where 'down' is. You can use this to correct drift in the integrated gyro angle EXCEPT for rotation around the gravitational vector. That's why people also add magnetometers to correct for that.

    The downside of the accelerometer is that it also measures the acceleration of your copter. So if you move quickly, it will have a wrong picture of where 'down' is. Smart filters (Kalman / extended Kalman) are used to neglect acceleration data during fast movements.

     

    To get back to your question: the most versatile solution is to use Invensenses overprized MPU9150 (available on Sparkfun breakout board). It features a 3D accelerometer, gyroscope AND magnetometer. With the default settings you can read out the raw sensor values, but with special firmware (google for Pansenti MPU9150) you can get orientation data out of the device.

     

    To get even more back to your question:

    You say you're only interested in 'values' in X and Y directions. But what 'values' do you need? linear displacement? Change in rotation? With respect to what? If you've got that clear you can probably find out easier which sensor fits your basic needs.....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • vsluiter
    0 vsluiter over 13 years ago

    Barry,

     

    You'll probably need both; the gyroscope measures angular velocity (degrees/second), which is good for maintaining a constant angle. You just need to integrate the angular velocity to get the angular position, and that way you can keep the camera at a constant angle with respect to your copter.

    However, that's probably not good enough; the gyros have a small error that adds up while integrating (because integrating boils down to adding up samples), and you probably want to keep the angle constant with respect to the earth, not the copter. That's why people use accelerometers. With an accelerometer you can determine the gravitational vector, i.e., you know where 'down' is. You can use this to correct drift in the integrated gyro angle EXCEPT for rotation around the gravitational vector. That's why people also add magnetometers to correct for that.

    The downside of the accelerometer is that it also measures the acceleration of your copter. So if you move quickly, it will have a wrong picture of where 'down' is. Smart filters (Kalman / extended Kalman) are used to neglect acceleration data during fast movements.

     

    To get back to your question: the most versatile solution is to use Invensenses overprized MPU9150 (available on Sparkfun breakout board). It features a 3D accelerometer, gyroscope AND magnetometer. With the default settings you can read out the raw sensor values, but with special firmware (google for Pansenti MPU9150) you can get orientation data out of the device.

     

    To get even more back to your question:

    You say you're only interested in 'values' in X and Y directions. But what 'values' do you need? linear displacement? Change in rotation? With respect to what? If you've got that clear you can probably find out easier which sensor fits your basic needs.....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to vsluiter

    I found this web page to be very helpful.  It helps explain the values read from the acceleration and gyroscope sensors, and how they are combined.

    http://www.starlino.com/imu_guide.html