Sensors
  • Technologies
  • More
Sensors
Sensor Forum Nightlight Photocell located away from the LED
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 351 subscribers
  • Views 652 views
  • Users 0 members are here
Related

Nightlight Photocell located away from the LED

e14 Contributor
e14 Contributor over 13 years ago

I am new to electronics.

I want to set up a Photocell with a night light (LED).  The unique aspect is that I want the Photocell to be four feet (4') away from the LED.  Where the night light is locted, it is always dark (so the night light stays on); however, the room is light -- so, I want the photo cell to be about four feet (4') away from the night light (the photocell will be located where is will be affected by the actual light in the room).

Is it possible to put the photocell four feet (4') away?  If so, what kind of wire do I use?

Thanks for your input!

Richard

  • Sign in to reply
  • Cancel
Parents
  • mraureliusr
    0 mraureliusr over 13 years ago

    As Doug said, you basically just need to ensure that you match the original connections exactly. I would recommend going with a fairly small gauge wire, and I would also recommend at least heat shrinking each end for a bit of strain relief, not to mention it'll look a bit better image

     

    Buying some sort of shielded wire is a good idea as well. Actually you can probably easily harvest some from some old electronics. Look for wire that contains two or more smaller wires withing -- multicondutor wire, we call it.

     

    Good luck! Feel free to ask more questions, if you have design-related questions be sure to post pictures.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jvdberg@ieee.org
    0 jvdberg@ieee.org over 13 years ago in reply to mraureliusr

    Hi Richard, Like Doug and others already wrote, it is possible to extend the wires. Most plug in night lights are not isolated from the mains voltage. For safety the extension wire and the connections at the light and at the sensor must have reliable insulation.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jvdberg@ieee.org
    0 jvdberg@ieee.org over 13 years ago in reply to mraureliusr

    Hi Richard, Like Doug and others already wrote, it is possible to extend the wires. Most plug in night lights are not isolated from the mains voltage. For safety the extension wire and the connections at the light and at the sensor must have reliable insulation.