Sensors
  • Technologies
  • More
Sensors
Sensor Forum Help: Solution for Detecting the No of persons sitting on a seat
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 57 replies
  • Answers 1 answer
  • Subscribers 355 subscribers
  • Views 8554 views
  • Users 0 members are here
Related

Help: Solution for Detecting the No of persons sitting on a seat

e14 Contributor
e14 Contributor over 12 years ago

Hi,

I need help on detecting the number of persons sitting on a seat of short length. The way of sitting is same like we sit on a bike.. Please share your ideas after that i will discuss the ways implemented so far. I am limited by the knowledge in sensors Help will be appreciated.

  • Sign in to reply
  • Cancel

Top Replies

  • michaelwylie
    michaelwylie over 12 years ago in reply to e14 Contributor +2
    This sounds like an EE senior design project to me, am I correct? Edit: Maybe too advanced for a senior design, so a Master's Thesis?
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to vsluiter +2
    First things First:: Please dont worry about you doing my homework i have came to this forum only after getting stalled. Moreover iam a Research Student, School times have passed things arent proving that…
  • vsluiter
    vsluiter over 12 years ago in reply to e14 Contributor +1
    Can you tell a bit more about your application? Why can't you use load sensing? Please give more information on what your constraints are. If you can't use load sensing, you'll have to use a camera and…
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Thanks For the reply..

    The project is Detecting the number of persons seated on a Two wheeler.

    1> We cant use the load sensor is because the weight of the persons seated can vary largely that makes it non-applicable.

    2> I had thought to use a switch Case array- But limited with the i/o pins of the controller. In this i had thought to pogram it as such that it will make a profile of the person as per the pattern generated by the seated area and the gaps between the persons can be used to detect the persons seated.

    3> Ideas are welcomed

    I dont need to specify the nature of environment, Just a Bike seat

    Thanks Regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 12 years ago in reply to e14 Contributor

    Is this a bicycle or a motorcycle seat - I don't see how a bicycle seat fits more than one.

    Is there more than one seat?

    If it is a motorcycle, there may not be a gap between riders.

    Is there room to put an optical (light interruption) sensor at each seating position?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dougw
    0 dougw over 12 years ago in reply to e14 Contributor

    Is this a bicycle or a motorcycle seat - I don't see how a bicycle seat fits more than one.

    Is there more than one seat?

    If it is a motorcycle, there may not be a gap between riders.

    Is there room to put an optical (light interruption) sensor at each seating position?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • billpenner
    0 billpenner over 12 years ago in reply to dougw

    Please give the maximum number of people and. the dimensions of the seat  If you expect a meaningful answer, you must give related data.

    Bill