Sensors
  • Technologies
  • More
Sensors
Sensor Forum Help: Solution for Detecting the No of persons sitting on a seat
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 57 replies
  • Answers 1 answer
  • Subscribers 355 subscribers
  • Views 8590 views
  • Users 0 members are here
Related

Help: Solution for Detecting the No of persons sitting on a seat

e14 Contributor
e14 Contributor over 12 years ago

Hi,

I need help on detecting the number of persons sitting on a seat of short length. The way of sitting is same like we sit on a bike.. Please share your ideas after that i will discuss the ways implemented so far. I am limited by the knowledge in sensors Help will be appreciated.

  • Sign in to reply
  • Cancel

Top Replies

  • michaelwylie
    michaelwylie over 12 years ago in reply to e14 Contributor +2
    This sounds like an EE senior design project to me, am I correct? Edit: Maybe too advanced for a senior design, so a Master's Thesis?
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to vsluiter +2
    First things First:: Please dont worry about you doing my homework i have came to this forum only after getting stalled. Moreover iam a Research Student, School times have passed things arent proving that…
  • vsluiter
    vsluiter over 12 years ago in reply to e14 Contributor +1
    Can you tell a bit more about your application? Why can't you use load sensing? Please give more information on what your constraints are. If you can't use load sensing, you'll have to use a camera and…
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I think it can be done with a weight sensor. Start with stationary weight without people and check if it gets heavier in steps (like minimum 10 kilo). I think 1 person will be added at a time. Should look like this:

     

    Start with 250 kilo, add 50 kilo (1 person), add 30 kilo (2 persons) etc.

     

    There should be some form of timeout to calculate the results. You could draw a graph to see this working.

     

    This can be done with an inductive sensor (http://www.ti.com/tool/ldc1000evm).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 12 years ago in reply to e14 Contributor

    Start with 250 kilo, add 50 kilo (1 person), add 30 kilo (2 persons) etc.

    You haven't been to the Pacific Islands.

     

    I agree; we shouldn't make his homework.

    Strangely we seem to attract these queries ...image

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to mcb1

    250 is the initial weight of motor cycle as example.  You can start with 0.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 12 years ago in reply to e14 Contributor

    250 is the initial weight of motor cycle

    Yes that wasn't the figure I was referring to.

     

    Its very hard for the scooter to measure itself, but the initial scooter weight is not a factor anyway...

     

    This shows how this won't work.

    Scenario1       Person A weighs 40kg, person B weighs 40kg, luggage weighs 10kg. Luggage is picked up and carried after A and B are seated.

    Scenario 2      Person A weighs 40kg, person B weighs 40kg, person C weighs 10kg. They get on last.

    Scenario 3      Person A weighs 50kg, person B weighs 30kg, person C is being carried by person B and weighs 20kg. and gets on at the same time.

     

    Placing a load sensor in the seat only works if they sit on the seat, and the spring rates are non linear, so unless you modify the spring mounts (front and rear) you're likely to have to calibrate the sensor.

    Once you do that you have a way to 'bypass' it.

     

    The reality with any of these methods is there is a way to overcome them and humans tend to find the way.

     

    Now the other question.

    What do you do in an emergency when it would be desirable to be able to load the scooter with 4 (or more) people as the roads are damaged so other vehicles can't get through, and you need to get them to emergency care.?

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mcb1
    0 mcb1 over 12 years ago in reply to e14 Contributor

    250 is the initial weight of motor cycle

    Yes that wasn't the figure I was referring to.

     

    Its very hard for the scooter to measure itself, but the initial scooter weight is not a factor anyway...

     

    This shows how this won't work.

    Scenario1       Person A weighs 40kg, person B weighs 40kg, luggage weighs 10kg. Luggage is picked up and carried after A and B are seated.

    Scenario 2      Person A weighs 40kg, person B weighs 40kg, person C weighs 10kg. They get on last.

    Scenario 3      Person A weighs 50kg, person B weighs 30kg, person C is being carried by person B and weighs 20kg. and gets on at the same time.

     

    Placing a load sensor in the seat only works if they sit on the seat, and the spring rates are non linear, so unless you modify the spring mounts (front and rear) you're likely to have to calibrate the sensor.

    Once you do that you have a way to 'bypass' it.

     

    The reality with any of these methods is there is a way to overcome them and humans tend to find the way.

     

    Now the other question.

    What do you do in an emergency when it would be desirable to be able to load the scooter with 4 (or more) people as the roads are damaged so other vehicles can't get through, and you need to get them to emergency care.?

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to mcb1

         "The reality with any of these methods is there is a way to overcome them and humans tend to find the way."

     

    Mark, if you think this way you will never find a solution. You are also making the problem bigger than it is. Scenario 1, two people and luggage should also be too much for a motorcycle. Scenario 2 works fine.

     

    It is possible to limit the speed instead of a blocking situation. Or any other annoying adjustment.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • billpenner
    0 billpenner over 12 years ago in reply to e14 Contributor

    Finally It seems that you have a ride on a cycle of some kind that you don't want more than one person on. Could you put a row of temp,  pressure, light, etc. on the seat or frame to get a gradient or peak value of the sensors. There should be a peak for each of the passengers.

    Bill