Sensors
  • Technologies
  • More
Sensors
Sensor Forum Help: Solution for Detecting the No of persons sitting on a seat
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 57 replies
  • Answers 1 answer
  • Subscribers 355 subscribers
  • Views 8572 views
  • Users 0 members are here
Related

Help: Solution for Detecting the No of persons sitting on a seat

e14 Contributor
e14 Contributor over 12 years ago

Hi,

I need help on detecting the number of persons sitting on a seat of short length. The way of sitting is same like we sit on a bike.. Please share your ideas after that i will discuss the ways implemented so far. I am limited by the knowledge in sensors Help will be appreciated.

  • Sign in to reply
  • Cancel

Top Replies

  • michaelwylie
    michaelwylie over 12 years ago in reply to e14 Contributor +2
    This sounds like an EE senior design project to me, am I correct? Edit: Maybe too advanced for a senior design, so a Master's Thesis?
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to vsluiter +2
    First things First:: Please dont worry about you doing my homework i have came to this forum only after getting stalled. Moreover iam a Research Student, School times have passed things arent proving that…
  • vsluiter
    vsluiter over 12 years ago in reply to e14 Contributor +1
    Can you tell a bit more about your application? Why can't you use load sensing? Please give more information on what your constraints are. If you can't use load sensing, you'll have to use a camera and…
Parents
  • jw0752
    0 jw0752 over 12 years ago

    Hi Bashir

    Here is an idea. I am going to assume that only one person at a time can add their body to the bike. We are going to put a pressure sensor, like an bladder into the seat and connect it to a pressure sensor. We are not going to be concerned with specific pressures as people sit on the seat but rather we will detect pressure plateaus. We will use a micro processor to count the pressure plateaus. For example the first person sits on the seat and a max pressure, that is stable for a second or two, is detected. The next person sits on the seat and a second pressure plateau is detected, which is also stable for a second or two. Finally if a third or fourth pressure plateau is detected then the microprocessor disengages the ignition. You would have to program the processor to test for any pressure that falls within a range plus or minus "x" Kpa for a second or two. If a second greater pressure is then added and stabalizes for a second or two we have our second person. Then if a third higher pressure is obtained we have our prevent ignition point. You will have to make sure that there is a fail safe so that once the bike is started and moving that the ignition shut down can not happen as the bike and people bounce over rough terain. Perhaps a timer that takes the shutdown out of the picture once the bike has been started and moving for 5 seconds. Good luck

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 12 years ago

    Hi Bashir

    Here is an idea. I am going to assume that only one person at a time can add their body to the bike. We are going to put a pressure sensor, like an bladder into the seat and connect it to a pressure sensor. We are not going to be concerned with specific pressures as people sit on the seat but rather we will detect pressure plateaus. We will use a micro processor to count the pressure plateaus. For example the first person sits on the seat and a max pressure, that is stable for a second or two, is detected. The next person sits on the seat and a second pressure plateau is detected, which is also stable for a second or two. Finally if a third or fourth pressure plateau is detected then the microprocessor disengages the ignition. You would have to program the processor to test for any pressure that falls within a range plus or minus "x" Kpa for a second or two. If a second greater pressure is then added and stabalizes for a second or two we have our second person. Then if a third higher pressure is obtained we have our prevent ignition point. You will have to make sure that there is a fail safe so that once the bike is started and moving that the ignition shut down can not happen as the bike and people bounce over rough terain. Perhaps a timer that takes the shutdown out of the picture once the bike has been started and moving for 5 seconds. Good luck

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • shabaz
    0 shabaz over 12 years ago in reply to jw0752

    Agree, also the fail safe is a good idea.

    I get the feeling though that some things shouldn't be solved by electronics, and could be solved by other means (e.g. change mindsets like how drink-driving has plumetted over the years).

    There could be an emergency where several people did need to get on a bike, and then the electronics would prevent that, so this seems wrong :-(

    One project I knew considered licensing, but we removed any software lock on the product because there was always the risk that someone might need to use it in an emergency. Not sure it's easy to sleep at night knowing there is this risk with a product one rolls out. So it was accepted that there would be some abuse, and the lockout function was removed.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to jw0752

    @John Wiltrout : This case is already discussed as taking weight sensors and detecting the concentration points. Please elaborate the Bladder concept if it uses only a single sensor then it can work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to shabaz

    @shabaz I agree but some times just waiting for things to happen and if they happen can be quite boring except when you provide government a tool to act to this. I consider these thoughts only once i am sure i have the perfect solution to make such a thing after that only i think whether to implement it or not. Before even making if i think of its disadvantages i would end up doing nothing.

    The programming part can be manipulated in any direction ways can be devised that will allow to put the system in sleep in case of emergency.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 12 years ago in reply to e14 Contributor

    Hi Eeshan,

     

    That's good, just wanted to be sure you've checked it off. The project I saw, had spent a lot of time and effort in the lockout, only to remove it all entirely because it wasn't practical/usable for social reasons as John says.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 12 years ago in reply to e14 Contributor

    The bladder is an air or liquid filled bag that is under the upholstery of the seat. When someone sits anywhere on the seat the bag is squeezed which increases the pressure which in turn is sensed by a single pressure sensor. If a second person sits on the seat the bag is squeezed more increasing the pressure. If someone sits on someone else's lap the bag is squeezed more and the pressure increases. We do not have to worry about how much people weigh as we are not looking at any specific weights but only at stable pressure ranges that are above the unloaded pressure. When the microcomputer detects a pressure in the bladder that is above the base level it will count one person. When a second relatively stable pressure is detected it will count two people and if there is a third relatively stable higher pressure level we have counted our third person. This will not protect a situation where a mother with a child on her back gets on the bike as our sensor/microprocessor will see only the addition of one mass but if the mother gets on and then the child climbs into her lap it will detect the child. By counting stable pressure levels we can illiminate the complication of trying to estimate weights or compensate for the difference in boddy shapes and sizes. Even if people put some of their weight onto foot pegs or the ground, by detecting maximum pressure plateaus we can determine that only one person is being sensed by programming the correct code into the microprocessor. I hope this clarifies my idea.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to jw0752

    John, that's exactly like I said. But instead using pressure I suggested measuring movement using a metal plate and induction. Both solutions need some form of calibration.

     

    Elbert.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 12 years ago in reply to e14 Contributor

    Hi Elbert,

     

    I believe that you may be missing my point. The method I am suggesting would also work with your sensor but instead of looking at absolute values I want to look at the rate of chage of the sensor measurements. If we take 100 sensor readings a second and we compare each sensor reading to the average of the last 100 we will know when the mass has been put on the seat as we will see an increase in the numbers and then a leveling off of the numbers as the person comes to rest on the seat. We don't care if the person weighs 20 Kg or 80 Kg just that the readings have gone up and then stabalized. The secont person will cause the sensor reading to again increase to a average higher level and then stabalize at the higher value. The micro processor can keep track of these steps of increased mass on the sensor. When the count exceeds two processes of going up and stabalizing the micro processor can do what it needs to do. With this method no calibration or estimation of a persons average weight needs to be taken into account. The reason I chose the system with a pressure bladder in the seat is that my experience in more in pneumatics and I have worked with this type of system before. You are likely much better with variable inductances and could undoubtedly rough out a system using those sensors better than me. I believe my idea will work in a laboratory environment. Whether it can be tweeked to work in the real world is another question. If I was doing the project I probably would not mess with cutting the ignition but rather have the sensor illuminate a warning sign about the danger of more than 2 riders and let the driver make his own decision.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kas.lewis
    0 kas.lewis over 12 years ago in reply to jw0752

    If you are looking for movement, picking up a bag or anything would cause your "stabilizing counter" to increase therefore someone picking up two bags would appear as three people.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • billpenner
    0 billpenner over 12 years ago in reply to kas.lewis

    This has grown into quite a discussion. In my opinion, measurement of change in sensor value is by far the best solution. Suggested by many in the discussion primarily as John Wiltrout suggested. Just an additional tweak, How about a using an ultrasonic distance sensor mounted on the bottom of the bike centered between the wheels. Simple, easy to detect difference in weight (distance to the ground) easy interface to a microprocessor, one sensor with no calibration, only looking for stabilization. One demerit I can think of is if the kickstand was down when the passengers mounted, then when the weight was taken off the kickstand the sensor would register another passenger. Possibly corrected by a switch on the kickstand to prevent evaluation for the next x milliseconds?

    Bill

     

    RE: Kas

    Maybe set a minimum increase. That is recognize only a change of xx representing say more than 50 Lbs?+

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 12 years ago in reply to kas.lewis

    Hi Kas,

    You make an excellent point. these are some of the hard side effects that will have to be solved if the idea moves out of the lab and into the street. Part of the fun of a discussion like this is seeing if we can come up with a solution. How would you engineer a fix for the cyclist that wants to load two bags of groceries onto his bike before he heads home?

    John