Sensors
  • Technologies
  • More
Sensors
Sensor Forum Same Methane sensors works differently!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 351 subscribers
  • Views 1320 views
  • Users 0 members are here
  • mq4
  • methane
  • mq
  • connections
  • arduino
  • sensor
Related

Same Methane sensors works differently!

e14 Contributor
e14 Contributor over 11 years ago

Hello everyone,

I'm making a project with two Arduino Yùn which acquire Methane through MQ-4 gas sensors.

I've built 3 couple of circuits to let them work correctly (using resistance of 20 Kohms) but in each of the three tests one sensor gave 900 parts for million, instead the other almost 300. Obviously they were in the same room, very close to each other and not in direct presence of warm or heat sources.

The scheme of the connections is:

Sensor PINS:

 

      A       E

   B             F

      C      G

 

E,F,G to 5 Volts D.C.

A to A0 (Analog0 pin)

B to GND (Ground pin)

C to 20Kohm resistance then connected to the GND pin

What could be the reason for this difference?

  • Sign in to reply
  • Cancel
  • clem57
    0 clem57 over 11 years ago

    Why 20K resistor? I have another circuit similar and they use 10K See AirQualityMQ135 \ Learning \ Wiring

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to clem57

    Sensitively adjustment is necessary Please read https://www.sparkfun.com/datasheets/Sensors/Biometric/MQ-4.pdf

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to clem57

    The value of the resistor can be in the interval 2kOhms to 46kOhms as the official page says:

    "Resistance value of MQ-4 is difference to various kinds and various concentration gases. So,When using this components, sensitivity adjustment is very necessary. we recommend that you calibrate the detector for 5000ppm of CH4 concentration in air and use value of Load resistance ( RL) about 20KΩ(10KΩ to 47KΩ)."

     

    Still, I can't understand why all that difference of value if the connections are exactly the same... maybe the soldered parts of the circuit... or the quaity of the connections...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to e14 Contributor

    I would take a meter and check if the resistance is varying a great amount. That would explain.

    Clem