Sensors
  • Technologies
  • More
Sensors
Sensor Forum How to measure SO2, as by-product from the Claus process in refineries, cost-effective and most accurately (crowd sourced)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 2 answers
  • Subscribers 351 subscribers
  • Views 1848 views
  • Users 0 members are here
  • ppb
  • so2
  • dioxide
  • quality
  • sourcing
  • alphasense
  • sulphur
  • crowd
  • air
  • oxide
  • process
  • no2
  • no
  • parts-per-billion
  • refinery
  • nitro
  • claus
Related

How to measure SO2, as by-product from the Claus process in refineries, cost-effective and most accurately (crowd sourced)

e14 Contributor
e14 Contributor over 11 years ago

In my search for air quality sensors there doesn't seem much out there that could be as accurate as governments apparently are monitoring.

See this example from Kanagawa prefecture of Japan with apparent ppb accuracy per hour response time:

http://www.pref.kanagawa.jp/sys/taikikanshi/StationDailyReport/OfficeTimeReport0120501.htm

These government monitoring sites can be limited and do not always represent the reality due to local landscape and wind differences.

 

Crowd sourcing environmental quality data turned out to be an accepted watchdog of governments already.

See the efforts of Safecast global radiation monitoring for example. Even IAEA is kind of supportive:

http://www.fccj.or.jp/number-1-shimbun/item/330-the-crowdsourcing-genie-escapes-the-bottle/330-the-crowdsourcing-genie-e…

 

For air quality, specifically SO2 ppb levels can be an important indicator near refineries for potential other pollutive side products like NO, NO2 or NMHC.

You can smell SO2 at relatively low levels and it also has health effect at relatively low levels for people suffering from asthma.

Only this commercial sensor seems to be getting close although the response time is still a bit too slow to get in par with the mentioned Kanagawa example:

http://www.alphasense.com/WEB1213/wp-content/uploads/2013/12/SO2A4.pdf

 

Anyone at element14 who can shed a light on more accurate alternative solutions?

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 11 years ago in reply to shabaz +1
    Hi shabaz , When I would like to compare with existing Air Quality Monitoring stations something like 10ppb (not ppm) accuracy within 1 hour would be best. SO2 gets detected by my nose quite well when…
  • shabaz
    shabaz over 11 years ago in reply to e14 Contributor +1 suggested
    Hi Fred, I think you're looking at Figure 4 in the datasheet, but this isn't intended to show the response time, it is intended to show noise at different levels (and they tested at levels of 200, 160…
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to shabaz +1
    shabaz Thank you very much for your advise and nailing me on bad reading of the spec sheet That is why it is so useful to pose questions here and get answers from experienced people like you. cheers, …
Parents
  • shabaz
    0 shabaz over 11 years ago

    Hi Fred,

     

    What is the issue with the Alphasense device? Response time looks reasonable (20 sec to 90% level). I couldn't see the specific question you had - you want higher accuracy than the Alphasense device, or a faster response time since you mention that in your post?

    Is the Alphasense device not suitable?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to shabaz

    Hi shabaz,

     

    When I would like to compare with existing Air Quality Monitoring stations something like 10ppb (not ppm) accuracy within 1 hour would be best.

    SO2 gets detected by my nose quite well when I see 30ppb readings from a local monitoring station here in Yokohama, about 5 km from the refinery that is getting rid of it.

    This SO2A4 Alphasense sensor can do 20-40ppb in about 4000 ~ 5000 seconds only.

    Anything better than that will get lost in the noise if I read the document well at

    http://www.alphasense.com/WEB1213/wp-content/uploads/2013/12/SO2A4.pdf

    Maybe with noise filtering it could be used somehow? But still the response time wouldn't quite match.

     

    cheers,

    Fred

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 11 years ago in reply to e14 Contributor

    Hi Fred,

     

    I think you're looking at Figure 4 in the datasheet, but this isn't intended to show the response time, it is intended to show noise at different levels (and they tested at levels of 200, 160, 120, 80ppb and so on).

    They are showing noise in the time domain.

    The actual response time is the 't90' value on the first page (under Perfomance heading), which shows that from zero to 2ppm (i.e. 2000ppb) the time is less than 20 seconds to reach 90% of the value.

    The note in figure 4 indicates that noise is below 15ppb, with the opportunity to reduce that further with averaging algorithms.

    Accuracy is not indicated by the way. The datasheet figure 4 suggests that 20ppb is definitely detectable, but accuracy is not given as far as I can see (by the way, I've not used this sensor).

     

    If one needs accuracy from a single sensor to be comparable to government stations, then calibrated devices are presumably needed (I am no expert - but I suspect calibration from a lab is the way to achieve this, which is why the ones used in government stations are expensive).

    Indeed, if your aim is to hold governments accountable to specific levels, then they would only accept measurements from calibrated devices, so you have no choice anyway but to pay for expensive calibration regardless of the sensor.

     

    However, in theory there is another way (and you suggest it anyway in your post when you refer to crowd sourcing) - IoT can be empowering, because if you have measurements from multiple users, i.e. multiple sensors, then it becomes far harder to ignore trends if (say) 95% of those sensors in the IoT are suggesting levels are rising (and 5% have failed, for example). Basically stats will help. (I am no math expert in this area though). But I think a single accurate but non-calibrated sensor won't be acceptable, so cheap and multiple sensors are a way forward.

     

    The very innovative 'In the Air' challenge was predominantly established to help develop more and more of these types of IoT solutions by the way, by empowering people to develop and use long-term outdoor wireless sensor nodes and data collection and analysis in the cloud.

    There is a lot of information there on battery charging, low power processing, wireless comms, sensors and cloud platforms.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to shabaz

    shabaz

     

    Thank you very much for your advise and nailing me on bad reading of the spec sheet image

    That is why it is so useful to pose questions here and get answers from experienced people like you.

     

    cheers,

    Fred

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 11 years ago in reply to e14 Contributor

    Hi Fred,

     

    No problem at all, it is a very interesting topic!

     

    Thanks,

     

    Shabaz.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 11 years ago in reply to e14 Contributor

    Hi Fred,

     

    No problem at all, it is a very interesting topic!

     

    Thanks,

     

    Shabaz.