Sensors
  • Technologies
  • More
Sensors
Sensor Forum Responsivity of a photodetector
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 350 subscribers
  • Views 2353 views
  • Users 0 members are here
  • photomicrosensors
  • photodiode
  • photodetecors
  • photoresistor
Related

Responsivity of a photodetector

Abhi_shekkj27
Abhi_shekkj27 over 4 years ago
Hello
I am a PhD student working on photodetectors based on thin films.
I have fabricated a pn junction photodetector and have 5 LED sources (UV, IR, Blue etc) as radiation sources. 
Firstly, While calculating the Responsivity (R) of the device (R = Photocurrent / optical power) corresponding to each of those LED sources, I have made sure that the optical power of the sources is constant by ensuring the input electrical power given to the sources is the same. Is this assumption reasonable ?
Secondly, similar optical power would mean that the photon density of various LEDs are different, hence, i have kept photon density as a constant (thus optical powers are now different) and then i have calculated R.
I guess my question is, Does it matter whether I keep optical power a constant (or photon density a constant) while calculating Responsivity ?
  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 4 years ago +1
    I would suggest that optical power is not equal to electrical power, it more like the electrical power into the device generates both light and heat where the ratio of light to heat is the efficiency of…
  • dougw
    dougw over 4 years ago in reply to Abhi_shekkj27 +1
    UV emitters are easy since they are usually specified in mW / steradian. Converting steradians to square meters is pretty straightforward - just multiply the steradians by the square of the distance. …
Parents
  • dougw
    dougw over 4 years ago

    I would suggest that optical power is not equal to electrical power, it more like the electrical power into the device generates both light and heat where the ratio of light to heat is the efficiency of the device. So the optical power is the electrical power times the efficiency. I'm not sure how you are measuring photon density, but it usually is greatly influenced by the lenses in the setup.

    Assuming the responsivity is just the efficiency of the detector, as long as you can measure the input and the output of the detector it shouldn't matter what is held constant. Measuring the input optical power is tough as it involves figuring out how much optical energy is reaching all parts of the surface of the detector and none of the sources emits a uniformly distributed light pattern. The efficiency may also depend on the flux level.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 4 years ago

    I would suggest that optical power is not equal to electrical power, it more like the electrical power into the device generates both light and heat where the ratio of light to heat is the efficiency of the device. So the optical power is the electrical power times the efficiency. I'm not sure how you are measuring photon density, but it usually is greatly influenced by the lenses in the setup.

    Assuming the responsivity is just the efficiency of the detector, as long as you can measure the input and the output of the detector it shouldn't matter what is held constant. Measuring the input optical power is tough as it involves figuring out how much optical energy is reaching all parts of the surface of the detector and none of the sources emits a uniformly distributed light pattern. The efficiency may also depend on the flux level.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Abhi_shekkj27
    Abhi_shekkj27 over 4 years ago in reply to dougw

    Thank you . Just a follow up question

    Most LEDs come with brightness measured in millicandela. I learned to convert MCD into watts by first converting MCD into lumens and then into watts. For this, luminosity function was used which has various values between 0 and 1 . Now, if i have a UV LED for which the luminosity function value is zero, how can one convert MCD into watts ?

    Also, in the literature, usually authors mention watts/cm^2  of a LED given the luminous intensity/m^2 data. Any idea how to get luminous intensity/m^2 value?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 4 years ago in reply to Abhi_shekkj27

    UV emitters are easy since they are usually specified in mW / steradian. Converting steradians to square meters is pretty straightforward - just multiply the steradians by the square of the distance.

    MCD is a unit that only applies to visible light since it includes responsivity of the human eye. UV and IR light would all be 0 MCD regardless of power.