Sensors
  • Technologies
  • More
Sensors
Sensor Forum Angle detection
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 350 subscribers
  • Views 2672 views
  • Users 0 members are here
  • Outboard engine angle project..
Related

Angle detection

Lou_Blue
Lou_Blue over 4 years ago

I have a boat. The engine can be tilted up or down, coving a range of around 260° from fully up to fully down. I would like a more sophisticated sensor that is better than the 5 mercury tilt switches I'm currently using, which works pretty well. This is useful for fuel efficiency and shallow water hazards.

Is there an upgrade available that I can fit in my engine?

  • Sign in to reply
  • Cancel

Top Replies

  • colporteur
    colporteur over 4 years ago +2
    Your post has an angle theme so in the interest of community promotion there are two RoadTest that might give some insight. /products/roadtest/rt/roadtests/561/mps_magnetic_angle_p /products/roadtest…
  • robogary
    robogary over 4 years ago +1
    Are you asking if there is a commercially available alternative for engine positioning system and indication ? Are you looking for an infinitely adjustable angle position control ? Not sure this is the…
  • michaelkellett
    michaelkellett over 4 years ago +1
    This seems a very wide range of tilt angle, on my last (long time ago) power tilt outboard I think the range was about 90 degrees. Can you provide some pictures. My experience of boats suggests that…
Parents
  • robogary
    robogary over 4 years ago

    Are you asking if there is a commercially available alternative for engine positioning system and indication ?  Are you looking for an infinitely adjustable angle position control ? Not sure this is the best place to ask that question. How is the engine tilt activated, is it manually adjusted to the 5 engage the tilt switches as indication ? Do you select one of 5 positions for a controller to move the engine to that position ?  A sensor would be required to show engine angle relative to the boat. A mechanically activated potentiometer or an absolute encoder would serve that purpose, maybe even a simple quad encoder with a home switch. The control system then could do a position indication, or next step up, position controller.     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • robogary
    robogary over 4 years ago

    Are you asking if there is a commercially available alternative for engine positioning system and indication ?  Are you looking for an infinitely adjustable angle position control ? Not sure this is the best place to ask that question. How is the engine tilt activated, is it manually adjusted to the 5 engage the tilt switches as indication ? Do you select one of 5 positions for a controller to move the engine to that position ?  A sensor would be required to show engine angle relative to the boat. A mechanically activated potentiometer or an absolute encoder would serve that purpose, maybe even a simple quad encoder with a home switch. The control system then could do a position indication, or next step up, position controller.