Sensors
  • Technologies
  • More
Sensors
Sensor Forum Alternative approach to water leak detection
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 350 subscribers
  • Views 3736 views
  • Users 0 members are here
  • i2c
  • acoustic engineering
  • sensor
Related

Alternative approach to water leak detection

microphonon
microphonon over 4 years ago

Hello everyone, this is my first post here. For the past eight years, I have been developing an acoustic approach to water leak detection that can be located remotely from plumbing lines. It combines the principles of glass breakage and smoke detectors. The tech works very well so I am now trying to determine if there is a market for it. The design (hardware and firmware) is completely open source. It is listed as a pre-launch product on Crowd Supply. All information and details can be found at the following link:

https://www.crowdsupply.com/microphonon/aquaping

I would be interested in any comments or questions.

Mike H

  • Sign in to reply
  • Cancel

Top Replies

  • microphonon
    microphonon over 3 years ago +3
    Update: The Crowd Supply campaign for the acoustic leak sensor was successful. A production run has completed and units are being shipped to backers in 17 US States and 7 countries.
  • microphonon
    microphonon over 4 years ago in reply to kmikemoo +2
    Thanks for the comments. The intended use case is not as a handheld tool or plumber accessory, which is what I think you're suggesting. It's designed to be deployed as an automated, remote, low-power wireless…
  • shabaz
    shabaz over 4 years ago +1
    Hi, It sounds very useful, and I will probably order one when it's on Crowdsupply, or try to build one, to try it out. Since it is designed for high frequency sounds, perhaps the source code could…
Parents
  • shabaz
    shabaz over 4 years ago

    Hi,

    It sounds very useful, and I will probably order one when it's on Crowdsupply, or try to build one, to try it out.

    Since it is designed for high frequency sounds, perhaps the source code could also be one day extended to detect other anomalies with high freq content too, e.g. maybe glass smashing, or shots.

    A big hurdle for adoption would likely be the microphone I bet, but since you have a hardware filter, that provides a good amount of reassurance. However if removing the surround from the mic, or some other quick hack, could cause speech to be sensed (even at low amplitude), you might also want to show things like (say) if the microcontroller doesn't have the resources to capture or forward speech. Probably some customers would also want to be sure the processor could not run unauthorized code. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 4 years ago

    Hi,

    It sounds very useful, and I will probably order one when it's on Crowdsupply, or try to build one, to try it out.

    Since it is designed for high frequency sounds, perhaps the source code could also be one day extended to detect other anomalies with high freq content too, e.g. maybe glass smashing, or shots.

    A big hurdle for adoption would likely be the microphone I bet, but since you have a hardware filter, that provides a good amount of reassurance. However if removing the surround from the mic, or some other quick hack, could cause speech to be sensed (even at low amplitude), you might also want to show things like (say) if the microcontroller doesn't have the resources to capture or forward speech. Probably some customers would also want to be sure the processor could not run unauthorized code. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • microphonon
    microphonon over 4 years ago in reply to shabaz

    Thank you for the comments and questions. Glass breakage and gunshots are examples of short duration, impulse acoustic events. To capture these, the sensor must poll at a rate faster than the anticipated event duration, ie. likely approaching 1 kHz. This also requires the device to spend considerable time in active mode, which will consume power and affect battery life. Sensors are also available for these applications. The leak detector linked here targets persistent acoustics, which means the environmental sampling rate can be many times lower with much longer battery life. So these are really two different applications.

    An important design decision was to make speech capture impossible. The microphone is actually part of a bandpass Helmholtz mechanical filter centered at roughly 8 kHz with a Q of about 30. This is a followed by a 4th-order Sallen-Key high-pass analog electronic filter with cutoff at around 8 kHz. Even if the microcontroller was completely hacked, no intelligible conversation audio would ever reach it. A completely open-source approach allows the design to be inspected and verified that it cannot be used for eavesdropping.