Sensors
  • Technologies
  • More
Sensors
Sensor Forum Could you help me find issue in sensor circuit?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 20 replies
  • Subscribers 347 subscribers
  • Views 6291 views
  • Users 0 members are here
  • eagle
  • pcb
Related

Could you help me find issue in sensor circuit?

embeddedguy
embeddedguy over 3 years ago

I have designed a sensor with magnetometer and pressure sensor(ICP20100). After ordering the PCB and having done initial test, I could not find the ICP20100 on I2C bus(Address=0x63) while the other sensor is showing on the I2C bus.

Could you help me find the issue in my circuit diagram(Screenshot below)? as this could be the likely source of issue with the PCB. 

Note: As per the datasheet the CSB pin need to be high for I2C to active, hence I have removed the 10k resistor and short the pins.

The issue could be the capacitors C8/9 which needs to be low ESR as per datasheet. I ignored it because it was hard to find a caps which have this parameter listed in datasheet. So I used capacitors with same value and tolarances.

image

  • Sign in to reply
  • Cancel

Top Replies

  • Andrew J
    Andrew J over 3 years ago in reply to scottiebabe +3
    You’re right (of course). If the MPU6050 thinks it is the master for the downstream sensors, then it won’t be possible to enumerate these on the I2C bus from the system processor. What I don’t understand…
  • Andrew J
    Andrew J over 3 years ago +2
    Pin 6, ADO, defines the I2C address: low is 0x63; high is 0x64. This pin is connected to something off image and the component SJ4. Perhaps that is tied to ground somewhere which would seem ok, but if…
  • Andrew J
    Andrew J over 3 years ago in reply to Andrew J +2
    As a final thought, there are Arduino scripts thst enumerate the I2C bus to tell you what is on it. You could use, or adapt, that to check it isn’t hiding. In fairness though, I think the issue is how…
Parents
  • genebren
    genebren over 3 years ago

    This might be a minor thing, but in looking at your schematic, there is only a single RESV pin (with no pin number), while the PDF specification shows two RESV pins (pin 8 and 9).  Maybe the the linked schematic  (by scottiebabe ) is for a different version of this chip, but I would double check this part of the schematic and the library package for the ICP-20100.

    Also, the section of the schematic that you have included does not show all the power routing. Are all of the I2C chips being powered at 3.3V? With I2C being an open collector interface there should not be too much of an issue, unless some of the I2C devices are powered at higher voltages, then they might have logic level issues and not see logic high levels.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • genebren
    genebren over 3 years ago

    This might be a minor thing, but in looking at your schematic, there is only a single RESV pin (with no pin number), while the PDF specification shows two RESV pins (pin 8 and 9).  Maybe the the linked schematic  (by scottiebabe ) is for a different version of this chip, but I would double check this part of the schematic and the library package for the ICP-20100.

    Also, the section of the schematic that you have included does not show all the power routing. Are all of the I2C chips being powered at 3.3V? With I2C being an open collector interface there should not be too much of an issue, unless some of the I2C devices are powered at higher voltages, then they might have logic level issues and not see logic high levels.