Sensors
  • Technologies
  • More
Sensors
Sensor Forum NEED HELP with the ICM-20948 breakout board.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 347 subscribers
  • Views 5939 views
  • Users 0 members are here
  • accelerometer
  • icm-20948
  • sparkfun
  • magnetometer
  • gyroscope
  • icm
  • adafruit
  • vibration
Related

NEED HELP with the ICM-20948 breakout board.

irs
irs over 3 years ago

Hi, I have created a ICM 20948 breakout. The schematic is almost similar to the one available online, the only difference is that I have only inserted the I2C pins as I was only using them for the communication purpose. Now, after getting the PCB printed and embedding the components onto it the board is not working. I used a multimeter to observer voltages on different points SCL and SDA which are used in I2C so I observed a voltage of 3.2V. I also  used the multimeter to check the continuity on the board and the sensor. So , continuity was well established. 

I also used a Logic Analyzer to observe the i2C signals but, there was no data available.

Now anyone who has created and assembled the board. Can you please help me out. Just please check my schematic if it's right or not and what possible 

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 3 years ago +2
    Are you sure it's a working circuit? There's no decoupling capacitors near the ICM chip. Also, the ones near the voltage regulator are labeled 100pF. Are you sure that's correct? Photo of the assembled…
  • dang74
    dang74 over 3 years ago +1
    I am not 100% sure but my gut tells me that the level shifters made from the BSS138LT1G Moffetts can only operate in one direction with the 1.8V logic signal at the source being the input and the 3.3V…
  • baldengineer
    baldengineer over 3 years ago in reply to dang74 +1
    It looks like the BSS138LT 's max Vgs-thres is 1.5 volts.So, it would probably be marginal for a 1.8 volt system, but without scope measurements we won't know for sure.
Parents
  • baldengineer
    baldengineer over 3 years ago
    irs said:
    I also  used the multimeter to check the continuity on the board and the sensor. So , continuity was well established.

    For data signals like I2C, you really need to use an oscilloscope to see what is going on. A logic analyzer is useful to see if the signals are toggling but a scope will show you if there is a signal quality problem.

    You really need to see if both sides have activity and verify that both sides have a peak-to-peak voltage you expect.

    Schematic-wise, it looks like you did the level shifter correctly--assuming you schematic's pinout matches the pcb's footprint for the BSS138s.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • baldengineer
    baldengineer over 3 years ago
    irs said:
    I also  used the multimeter to check the continuity on the board and the sensor. So , continuity was well established.

    For data signals like I2C, you really need to use an oscilloscope to see what is going on. A logic analyzer is useful to see if the signals are toggling but a scope will show you if there is a signal quality problem.

    You really need to see if both sides have activity and verify that both sides have a peak-to-peak voltage you expect.

    Schematic-wise, it looks like you did the level shifter correctly--assuming you schematic's pinout matches the pcb's footprint for the BSS138s.