Sensors
  • Technologies
  • More
Sensors
Sensor Forum LCD sniffer for 12 pin custom LCD
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Subscribers 343 subscribers
  • Views 2639 views
  • Users 0 members are here
Related

LCD sniffer for 12 pin custom LCD

VikramSaharan
VikramSaharan over 3 years ago

Hello everyone 

I am trying to interface a TDS test pen with arduino. It has a 12 pin custom LCD. I want to get its LCD readings on serial monitor. I have no data sheet of the device under question.  Kindly help. 

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 3 years ago +3
    Is there any other interface available on that device? Maybe an unpopulated connector on the PCB? Or do you know what microcontroller is used, and what pins of that controller go to the LCD? If the LCD…
  • VikramSaharan
    VikramSaharan over 3 years ago in reply to Jan Cumps +1 verified
    This one has 12 pin lcd there is no any specification on main ic. A 8 pin another ic having marking ATMLH904 is also present
Parents
  • Jan Cumps
    0 Jan Cumps over 3 years ago

    Is there any other interface available on that device? Maybe an unpopulated connector on the PCB?
    Or do you know what microcontroller is used, and what pins of that controller go to the LCD?

    If the LCD has a driver IC, it may be (kind of) doable, because the signals will be digital.
    If the controller has the driver embedded (rare), the voltages on the interface pins may invert. Check that first with an oscilloscope.

    If you confirmed that the driver signals are digital 0/1 lines, you can start with the next activity:
    - use a digital analyser to capture communication, and try to relate it to what appears on the LCD. If you manage to solve that, you could build a gizmo, and write software to decode the LCD data into ascii and stream it over a serial.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • VikramSaharan
    0 VikramSaharan over 3 years ago in reply to Jan Cumps
    • image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • VikramSaharan
    0 VikramSaharan over 3 years ago in reply to Jan Cumps
    • image