Sensors
  • Technologies
  • More
Sensors
Sensor Forum How to detect vehicle sound at 100 m distance using microphone and Arduino?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 14 replies
  • Subscribers 345 subscribers
  • Views 1787 views
  • Users 0 members are here
Related

How to detect vehicle sound at 100 m distance using microphone and Arduino?

abhishekks
abhishekks over 1 year ago

Hello everyone,

I am working on a project where I need to detect the sound of vehicles (cars, heavy trucks) from a distance of around 100 m. The microphone will be placed in an open area on land, and the goal is to identify when a vehicle is approaching.

Currently, I am evaluating microphones like AOM-5024L-HD-R and CMA-4544PF-W, connected to a MAX9814 preamplifier module, with the output fed into an Arduino Uno ADC.

My questions are:

  1. What type of microphone is most suitable for long-distance vehicle detection (100 m)?
  2. How can I calculate whether the microphone output voltage will be sufficient for reliable detection at that distance?
  3. Should I use additional filters (e.g., low-pass or band-pass) to separate vehicle sound from background noise (wind, people, etc.)?
  4. Would I need a higher-gain preamplifier or a different approach (like a geophone or array microphone) for better detection?

Any advice, references, or design suggestions will be very helpful.

  • Sign in to reply
  • Cancel

Top Replies

  • beacon_dave
    beacon_dave over 1 year ago in reply to abhishekks +2
    If it is a narrow capture angle you could perhaps try a large diameter parabolic reflector with the mic placed at the focal point. It's surprising what you can hear with your ear at the focal point of…
  • michaelkellett
    michaelkellett over 1 year ago +1
    This can help you: https://calculator.academy/road-noise-calculator/ Then use the sound level to work out how much output from your microphone. You will have huge problems with wind noise and other…
  • beacon_dave
    beacon_dave over 1 year ago in reply to beacon_dave +1
    Depending on the application, a camera with motion tracking algorithm might also be worth considering as an alternative.
Parents
  • robogary
    0 robogary over 1 year ago

    Very intriguing project ! With no experience myself with the signal processing portion, Id like to learn more by asking questions that hopefully the community can help with.

    The microphone analog input of the sound source to Arduino has 2 properties: frequency bandwidth and amplitude. The amplitude for the Arduino input is 0-5v for 1023 counts. Your microphone detection of traffic at 100m is likely alot smaller amplitude than at 1m. Does the dynamic range of the signal provide digital resolution in Arduino , i.e. 50mV is 1 count ? 

    Traffic noise is likely low frequency- maybe as low as 30-50Hz, maybe to 500 Hz ? Analog filter would be good to get rid of unnecessary audio content.

    Do you envision to scan the analog input as fast as possible, or interrupt to create sampling comparable to 1 or 2 kHz ? 

    I could be making this task way overcomplicated, do you have some example code or library to convert the digital samples to a frequency spectrum ? I expect this library would be significant.

    I have played with a MSGEQ IC that uses a comparator ladder and filters to output bits based on frequency. 

    https://www.digikey.com/htmldatasheets/production/2071107/0/0/1/msgeq7.html?gclsrc=aw.ds&gad_source=1&gad_campaignid=120565755&gclid=Cj0KCQjw_rPGBhCbARIsABjq9cdKCctZg2WHu3NC_ZxKhzYaMPR5LzzfQyZzkXQYnzaytEZl5qho1fMaAieCEALw_wcB

    The Arduino code needed to scan & demultiplex is straightforward,  but you likely could not tell the difference between a truck at 100m or a duck at 1 m , without some knowledge of the frequency spectrum signature of the source. 

    Id like to understand more of the digital signal processing part, but particular to your project, maybe it better to focus on ground vibration for vehicle detection rather than audio. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • abhishekks
    0 abhishekks over 1 year ago in reply to robogary

    hi robogary,

    thanks for your knowledge.
    my first phase of project is to detect vehicle sound (ex: Innova car) from distance moving towards mic. output should be some voltage level and while moving towards Mic voltage level should increase.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • abhishekks
    0 abhishekks over 1 year ago in reply to robogary

    hi robogary,

    thanks for your knowledge.
    my first phase of project is to detect vehicle sound (ex: Innova car) from distance moving towards mic. output should be some voltage level and while moving towards Mic voltage level should increase.