Sensors
  • Technologies
  • More
Sensors
Sensor Forum Is there any sensor that can detect melting of electrical wires
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 349 subscribers
  • Views 372 views
  • Users 0 members are here
  • sensor
Related

Is there any sensor that can detect melting of electrical wires

manojroy123
manojroy123 1 month ago

Is there any sensor that can detect melting of electrical wires. The smell of melting electrical wire is disgusting.

  • Sign in to reply
  • Cancel

Top Replies

  • robogary
    robogary 1 month ago +1
    Like a smoke detector ?
  • cstanton
    cstanton 1 month ago +1
    manojroy123 said: Is there any sensor that can detect melting of electrical wires There are options. Consider the following that would be associated with this happening: - Temperature increase -…
  • BigG
    BigG 1 month ago +1
    Suggest a Metal-Oxide Semiconductor (MOS) gas sensors tuned for TVOCs. Sensirion SGP40 / SGP41 is a good bet. Otherwise, Bosch BME680. No doubt, other cheaper analog MOS sensors could be used too.
Parents
  • cstanton
    cstanton 1 month ago
    manojroy123 said:
    Is there any sensor that can detect melting of electrical wires

    There are options. Consider the following that would be associated with this happening:

    - Temperature increase

    - Resistance change

    - Particulate matter in the air

    Also consider:

    - What is happening to create this scenario in the first place?

    - Can the issue be prevented with proper requirements analysis and parts used?

    - What actions do you want to happen when it's detected?

    The recommended solution is determined by what level of voltage and current you're working with.

    If we're talking about working with a microcontroller, and voltages between 1.8v and 20v - then maybe you should be looking at using appropriate wiring before putting in a solution that "detects melted wires". Education and prevention is better than detection.

    If we're talking about reacting to a badly designed graphics card, then yeah, maybe you want to do voltage and current sensing and put some 'smarts' on there:
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
    But if you're talking about 100v+ and mains equipment, well you should definitely be measuring more on prevention, cut off, and appropriate reaction and following electrical standards.

    With a little bit of what robogary says, like a smoke detector.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • robogary
    robogary 1 month ago in reply to cstanton

    Nice reply, the question itself was pretty vague and generic.

    There are several things for prevention that you mentioned. 

    Motors and their wires need overload and stalled motor protection. Transformers and their wires need overload and ioc protection.

    In some places ground fault detection may be needed.

    To manojroy123: regular maintenance is also important in a factory. Electrical connections need checked for tightness , check for signs of overheating either with a thermal gun or visual check, conductive lubrication on aluminum wires, sharp edges or wires touching metal boxes can chafe and short to ground.

    Ventilation / air flow maintained around electrical enclosure fans and heat sinks. 

    Avoid issues that cause wires to melt with circuit protection...

    ......And then a generous distribution of cameras and smoke detectors around the equipment. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • robogary
    robogary 1 month ago in reply to cstanton

    Nice reply, the question itself was pretty vague and generic.

    There are several things for prevention that you mentioned. 

    Motors and their wires need overload and stalled motor protection. Transformers and their wires need overload and ioc protection.

    In some places ground fault detection may be needed.

    To manojroy123: regular maintenance is also important in a factory. Electrical connections need checked for tightness , check for signs of overheating either with a thermal gun or visual check, conductive lubrication on aluminum wires, sharp edges or wires touching metal boxes can chafe and short to ground.

    Ventilation / air flow maintained around electrical enclosure fans and heat sinks. 

    Avoid issues that cause wires to melt with circuit protection...

    ......And then a generous distribution of cameras and smoke detectors around the equipment.