Sensors
  • Technologies
  • More
Sensors
Sensor Forum Looking for high temperature pressure sensor with 4-20mA output
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 351 subscribers
  • Views 1483 views
  • Users 0 members are here
Related

Looking for high temperature pressure sensor with 4-20mA output

DaveMcLaughlin
DaveMcLaughlin over 9 years ago

I am looking for a pressure sensor capable of working in ambient temperatures of up to 125 deg both the pressure port and the electronics/body section.

 

I've found a few that can do this. Some expensive but most of the ones I have found are too big. The limitation is on the body dimensions. Length can be anything but the max diameter is limited to 25mm.

 

Accuracy is max 0.15% for 2000 psi range bu ideally 0.1% is referred.

 

Calibrated across the full temperature range. Most of the ones I have found are max 80 deg C calibration so are well out at over 100 deg C.

  • Sign in to reply
  • Cancel
Parents
  • neilsroberts
    neilsroberts over 9 years ago

    Check out : pressure transmitter or Pressure sensors - WIKA United Kingdom

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • neilsroberts
    neilsroberts over 9 years ago

    Check out : pressure transmitter or Pressure sensors - WIKA United Kingdom