Sensors
  • Technologies
  • More
Sensors
Sensor Forum Process Data from Current Sensor
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 350 subscribers
  • Views 1387 views
  • Users 0 members are here
  • adc
Related

Process Data from Current Sensor

nicoloquinte
nicoloquinte over 8 years ago

Hello, im in a quandcopter project for a while now and I just figured out that I needed a current sensor on each Bldc Motor and one on the Geneal Battery Rail.

I wanted to go with a certain ACS712 "Fully Integrated, Hall Effect-Based Linear Current Sensor" but for that I need 5 ADC on my Microcontroller (ATSAM3X8E).

And, since I have 16 of them, thats ok !

 

But .... I dont know if I would use them :

  • I need a really precise data that I can look into later
  • I dont want noisy readouts ( 4x4A BLDCs + Buck converters + radio traciver ...)

 

should I use one ADC per Sensor, use the builts-in ADCs : that's enought, or dou you have any sugestions ?!

 

Thank you in advance

 

EDIT :

ok ... after checking the price, I dont know if thats really the component tha I need, if you know a cheaper one, that would be great !

  • Sign in to reply
  • Cancel

Top Replies

  • nicoloquinte
    nicoloquinte over 8 years ago in reply to genebren +2
    yeah. actually my bldc are generatin a lot of boise but,for example my antennas are enought away from them so their aren't a problem. therefore, I think i'll go with high precision resistors and 16 bit…
  • waelect
    waelect over 8 years ago +1
    I have recently used the ACS712 5A version and have a couple of higher current one, but I am concerned in the off the shelf version are a bit noisy. The chip is currently not recommended for new design…
  • nicoloquinte
    nicoloquinte over 8 years ago in reply to waelect +1
    Thank you for answer I didn't thought about using a resistor based sensor because I'm using lipo batteries to power the motors so It's why I went for these sensors but since I'm also monitoring the battery…
Parents
  • waelect
    waelect over 8 years ago

    I have recently used the ACS712 5A version and have a couple of higher current one, but I am concerned in the off the shelf version are a bit noisy. The chip is currently not recommended for new design, which suggests they will be discontinued. Looking at the manufacturers website there are some newer more precise version out there.

     

    Also depending on the amount of current you are drawing it is possible to place a simple voltage divider to reduce the output to suit a 3.3V ADC ref, although you will still need a 5V Vcc. The voltage divider method I used in a recent data-logger project and worked quite well.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • waelect
    waelect over 8 years ago

    I have recently used the ACS712 5A version and have a couple of higher current one, but I am concerned in the off the shelf version are a bit noisy. The chip is currently not recommended for new design, which suggests they will be discontinued. Looking at the manufacturers website there are some newer more precise version out there.

     

    Also depending on the amount of current you are drawing it is possible to place a simple voltage divider to reduce the output to suit a 3.3V ADC ref, although you will still need a 5V Vcc. The voltage divider method I used in a recent data-logger project and worked quite well.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • nicoloquinte
    nicoloquinte over 8 years ago in reply to waelect

    Thank you for answer

    I didn't thought about using a resistor based sensor because I'm using lipo batteries to power the motors so It's why I went for these sensors but since I'm also monitoring the battery voltages that's ok !

    But i dont think you can get an current se.sing with a voltage divider

     

    Nico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • waelect
    waelect over 8 years ago in reply to nicoloquinte

    The voltage divider was to use for the O/P of the ACS712 to knock down the 4.5/5V down to a lower voltage for the ADC. Even though it is noisy it is a very low cost solution. Just be mindful of the noise level. I had to add a filter on the output to reduce the noise.