Sensors
  • Technologies
  • More
Sensors
Documents Automotive MEMS sensor market to double
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: ALex
  • Date Created: 15 Oct 2009 2:22 AM Date Created
  • Last Updated Last Updated: 7 Oct 2021 12:38 AM
  • Views 658 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

Automotive MEMS sensor market to double

Source: http://www.engineerlive.com

 

iSuppli forecasts worldwide automotive MEMS sensor shipments will grow to 935.7 million units in 2012, rising at a compound annual growth rate (CAGR) of 12 per cent from 474.2 million units in 2006. Global auto MEMS sensor revenue will increase to $2.1 billion in 2012, increasing at a CAGR of 8 percent from $1.3 billion in 2006.


The automotive MEMS sensor segment consists of 26 established and emerging applications in chassis, power train and body electronics. Major product areas for automotive MEMS are inertial sensors, pressure sensors, flow sensors, infrared sensors and emerging sensors. These tiny devices perform a variety of safety, control and environmental functions, from airbag collision detection, to tire pressure monitoring, to engine management.


MEMS use many processes common in the silicon IC industry, but have either small moving parts or regions that sense different physical parameters.


“Driving the rapid growth of the automotive MEMS sensor market in the United States and Europe is a set of chassis safety-related mandates that makes compulsory the implementation of Electronic Stability Control (ESC) systems and tire-pressure monitors,” said Richard Dixon, senior analyst for MEMS at iSuppli. “Both applications significantly contribute to saving lives on the roads, and tire-pressure monitors also lower fuel consumption.”


Shipments of MEMS pressure sensors for Tire Pressure Monitoring Systems (TPMSs) are expected to reach 179 million units in 2012, up from 43.1 million in 2006. Shipments of MEMS inertial and pressure sensors used in ESC systems will increase to 158 million units in 2012, increasing at a Compound Annual Growth Rate (CAGR) of 17 per cent from 61.6  million units in 2006.


“These applications will allow the automotive MEMS sensor market to outgrow the automotive and car electronics segments over the next few years,” Dixon said.


“The US has led in the implementation of TPMS and ESC systems,” Dixon noted. “However, considerable lobbying by interest groups in Europe was recently rewarded by wide sweeping proposals on safety features, including ESC and TPMS. This will lead to considerable upside for suppliers because mandates support systems that require several MEMS sensors — four TPMS pressure sensors per car, a gyroscope with one of two low-g accelerometers in a cluster, and one or more brake pressure sensor per ESC system on average. For accelerometers and gyroscopes, mandates will more than double the number of sensors required.”

 

A second substantial market driver will emerge in 2009, when Europe’s stringent new emission–control regulations go into effect.


This will boost demand for powertrain pressure sensors, which are used for applications including optimizing engine operation and reducing particle emissions in diesels. Other healthy MEMS markets include high-g accelerometers for airbags. The fast growth of the Chinese market also is benefitting sensors.


“Mandates are reshaping the supply chain,” said Jérémie Bouchaud, principal analyst for MEMS at iSuppli. “In the case of ESC systems, transitioning rapidly from an expensive option to a standard function in just a few years will create a space for newcomers and threaten established second-tier suppliers.”


Bouchaud added that the market transparency brought by government mandates may herald greater commoditisation and price erosion in MEMS sensor products, as all suppliers provide products that conform to government specifications, and which accommodate a range spanning the most expensive to the cheapest available vehicle. This will reshape the competitive landscape for MEMS sensors due to increased competition, Bouchaud added.

  • market
  • mems
  • automotive
  • sensor