Sensors
  • Technologies
  • More
Sensors
Polls In what situation(s) should an optical sensor (reflective) be applied instead of an ultrasonic sensor?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: rscasny
  • Date Created: 22 Nov 2020 7:12 PM Date Created
  • Last Updated Last Updated: 11 Oct 2021 3:00 PM
  • Views 1285 views
  • Likes 2 likes
  • Comments 4 comments
Related
Recommended

In what situation(s) should an optical sensor (reflective) be applied instead of an ultrasonic sensor?

Poll Question: In what situation(s) should an optical sensor (reflective) be applied instead of an ultrasonic sensor?

  • sensor survey
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • DAB
    DAB over 5 years ago +5
    Difficult question to answer. If you go optical, you need to consider if you are using IR or visible light. In general, both sensor require a rather clean environment. Both are susceptible to particle…
  • michaelkellett
    michaelkellett over 5 years ago +3
    There isn't a single right answer here. I was about to vote for "distance is over 9 m" but then I thought of depth sounders, which both work under water and can sense over much greater distances than 9m…
  • genebren
    genebren over 5 years ago +3
    This is a simple question but the answer as always depends on many factors. The environment that you are operating in will influence your decision. Also cost can be a factor in you decision where ultrasonic…
  • kmikemoo
    kmikemoo over 5 years ago

    Other:  Cost and distance*.  Why the asterisk?  When I think of reflective sensors, I think of entry sensors and garage door safety circuits.  The distance (range) can be 3 feet for a personnel door up to 32 feet for a larger commercial garage door.  One size fits most.  Align the reflector back at the transceiver and you're up and running.  To quote Ron Popeil, "Set it and forget it."  The few ultrasonic sensors I've played with needed to be adjusted to respond correctly to the material being sensed.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 5 years ago

    This is a simple question but the answer as always depends on many factors.  The environment that you are operating in will influence your decision.  Also cost can be a factor in you decision where ultrasonic sensor cost can cost about 100 times more that optical sensors.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 5 years ago

    There isn't a single right answer here. I was about to vote for "distance is over 9 m" but then I thought of depth sounders, which both work under water and can sense over much greater distances than 9m. I don't know of any optical depth sounders !

     

    "Response speed must be fast" is the other possible, but how fast is fast ?

     

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 5 years ago

    Difficult question to answer.

    If you go optical, you need to consider if you are using IR or visible light.

    In general, both sensor require a rather clean environment. Both are susceptible to particle size obstructions.

     

    Definitely an application dependent decision.

     

    DAB

    • Cancel
    • Vote Up +5 Vote Down