Sensors
  • Technologies
  • More
Sensors
Quiz Strain Gauges Quiz
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: pchan
  • Date Created: 8 Aug 2022 5:41 PM Date Created
  • Last Updated Last Updated: 4 Jun 2024 7:46 PM
  • Views 17410 views
  • Likes 16 likes
  • Comments 69 comments
Related
Recommended

Strain Gauges Quiz

Strain gauges are used to measure strain in several applications, including aerospace, transportation, industrial and more. Test your knowledge with our quiz on strain gauges.

profile image
sponsored by sponsor logo

Quiz | Sensors | Industrial Automation | Resource | Transportation & Automotive

 

Strain Gauges Quiz
Strain Gauges Quiz Score 100% on our Strain Gauges Quiz and leave your feedback as a comment to earn this badge...

To earn the Strain Gauges Badge, score 100% on the quiz and leave your feedback on the quiz as a comment.

  • e14quiz
  • omega
  • strain gauges
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • maxpowerr
    maxpowerr over 4 years ago +1
    Is it possible to make a water level indicator on Strain gauges?
  • ralphjy
    ralphjy over 4 years ago +1
    Another informative quiz. I really haven't used strain gauges in any of my projects, so far...
  • navadeepganeshu
    navadeepganeshu over 4 years ago +1
    Interesting quiz! Is there a document to read through before attending this quiz? Used to see in earlier quizes,...
Parents
  • maxpowerr
    maxpowerr over 4 years ago

    Is it possible to make a water level indicator on Strain gauges?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • sxaw_VSP
    sxaw_VSP over 4 years ago in reply to maxpowerr

    Possible, but could be very troublesome depends on your application. If you only wish to know if the water hit the desired level or not, you can mount the gauge on a material that would slightly bent (but not over-bent as gauge has its max. elongation) and put it parallel to water surface at the desired level location. The gauge resistance would be altered when water hit the level & bend the substrate.

    Otherwise, you will need to use the gauge to measure the overall weight of the water, a.k.a use a load cell. You might also think using the water pressure but the difficulty is on finding the right substrate that is sensitive enough to curve the right amount when the pressure change while not breaking the strain gauge. Using a force sensitive resistor or piezoresistive film is much robust & cost effective in this case.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • sxaw_VSP
    sxaw_VSP over 4 years ago in reply to maxpowerr

    Possible, but could be very troublesome depends on your application. If you only wish to know if the water hit the desired level or not, you can mount the gauge on a material that would slightly bent (but not over-bent as gauge has its max. elongation) and put it parallel to water surface at the desired level location. The gauge resistance would be altered when water hit the level & bend the substrate.

    Otherwise, you will need to use the gauge to measure the overall weight of the water, a.k.a use a load cell. You might also think using the water pressure but the difficulty is on finding the right substrate that is sensitive enough to curve the right amount when the pressure change while not breaking the strain gauge. Using a force sensitive resistor or piezoresistive film is much robust & cost effective in this case.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • phoenixcomm
    phoenixcomm over 3 years ago in reply to sxaw_VSP

     sxaw_VSP  I don't know where you came up with "very troublesome depends on your application."This equipment has been used in aircraft for a few decades, 5 or 6 at least. You must have the inner and outer tubes drilled with large holes. the sensor is attached to a bridge and you're done! I have used this with water as well, it will work with any liquid.