Test & Tools
  • Technologies
  • More
Test & Tools
Blog Building Custom Helping Hands
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 12 Mar 2019 10:20 PM Date Created
  • Views 6258 views
  • Likes 20 likes
  • Comments 16 comments
  • bench vise
  • vise
  • helping hands
  • pcb_holder
  • helping_hands
  • vice
  • pcb holder
  • vises
Related
Recommended

Building Custom Helping Hands

shabaz
shabaz
12 Mar 2019

Introduction

For years I’ve been “helping hand”-less. Since I was a kid, the design of the classic helping hands has not really changed - it has stood the test of time, but just for lightweight tasks. For anything large/heavy, it all goes wrong.

 

Here’s one attempt at solving the problem.. it relies on cheap camera ball-heads and clamps, and a steel base. It can all be built in an hour or two, depending on how fancy a base is desired. Otherwise, it is all plug-and-play to assemble, like Lego.

image

 

This eight-minute video explains the project, and has some demo examples of it in action.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

This is the type of Helping Hands I was familiar with:

Image source: Google Imagesimage

 

Instead, I’ve been using a low-cost aluminium vice such as the one in the photo below to meet most of my needs, but occasionally I’d still like a helping-hands style tool, but a lot stronger, and customisable.

image

 

The bill-of-materials for this project is probably $40-50 in total, but there is the opportunity to reduce costs. It hinges on the fact that camera users often have very fancy equipment at their disposal! Searching on Amazon/Aliexpress revealed systems such as 'SmallRig’ which have components like 15mm diameter rods, and clamps. I purchased some to see if they could be useful. Any camera user will eventually have a ball head spare, so costs can be saved there too. There are very basic ones from Aliexpress for less than $5 but they are not very good : ( I used an old CB2.7 ball head, and a £12 SIOTI ball head from Amazon. Both are great.

 

For the base, I purchased an oval 15mm thick steel offcut for £3.99. Somewhere in the UK a large steel plate needed a shape cut out, and the factory sold the cut-outs on ebay.

 

It is low cost, has a reasonable footprint (168x99mm), and is very heavy (perhaps a kilogram) – perfect! I imagine factories in other countries will also sell offcuts for next to nothing. One person's scrap is another person's treasure..

image

 

There is a notch in the offcut where the cutting tool started, but that can be filled (Polyfilla, or even epoxy glueepoxy glue) if desired, or left as-is. Next, a ¼ inch UNC hole was tapped – this is the typical standard thread for consumer cameras. It is not essential, if the hole is untapped then epoxy glue could be used too.

image

 

I filed off the sharp edges and lightly hand-sanded it to get rid of the rust. It looked nice and industrial! Still, to go with the rest of the décor, I did paint it afterwards but that was unnecessary. Some rubber feet should be attached on the underside too.

 

Assembling It

There’s not much to say, it is trivial to connect it all together.

image

Materials

These were the main parts that I used, but there is plenty of scope for variation.

Item
1Steel base from ebay seller bitsandbobs332014
2Rubber feetRubber feet
31/4" to 1/4" Adaptor
4Ball Head
515mm Rod 150mm length
6Rod Clamp
7M12 to 1/4" Adaptor
8SmallRig Super Clamp

 

Customizing It

The possibilities are endless.. Another clamp arm could be attached if required. An LED light could be added. Custom grips could be 3D-printed to clip onto the current clamp jaws.

 

Using It

Check out the earlier video to see it in action – it’s surprising how many uses it has.

It can act as a PCB holder, although I still prefer using the aluminium flat vice for that.

image

 

It is extremely rigid, so things can be held at a distance, wherever it is easier to work.

image

 

It can hold heavy-ish antennas too!

image

 

I found that very large PCBs can be propped up.

image

 

Since the clamp has rubber grips, it is also very handy for holding oscilloscope probes in place. Also, it can help with holding large heavy cables close to connectors. I found it useful for soldering audio jacks!

image

 

Summary

I’m really happy how this simple project turned out. The entire unit is strong, and doesn’t easily tip while using it. In future I may try adding an LED light.

 

If you build any type of helping hands/clamp system, or have ideas for adaptations or attachments for it, it would be great to hear about them.

 

Thanks for reading!

  • Sign in to reply

Top Comments

  • 14rhb
    14rhb over 7 years ago +9
    Hi Shabaz, This is a great build and looks so much better than the standard croc-clip helping hands, well done. I bought myself some 1/4" UNC tap/die set years ago (so that I could make customised tripod…
  • ntewinkel
    ntewinkel over 7 years ago +9
    That's a REALLY nice design, Shabaz! I might have to try that for myself. I can likely get a chunk of heavy metal from my father-in-law. Nice how yours is perfectly shaped like that. I was about to order…
  • genebren
    genebren over 7 years ago +8
    shabaz, What a great idea (or series of ideas). The video was very good, I feel that you are quite good at capturing your ideas/explaining your process in your videos (far more comfortable than I feel…
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to genebren

    genebren  wrote:

     

    shabaz,

     

    ... (far more comfortable than I feel anywhere near a camera).   ...

    Gene

    The best way to get better at it is to make videos and publish them, even if you are uncomfortable with the result. Even if they are quirky and badly edited.

    You'll automatically get better, video by video. If you publish.

    • Cancel
    • Vote Up +8 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to genebren

    Hi Gene,

     

    Thanks!

    Those are really neat ideas. Regarding X/Y/Rotate, I remember a very old production system that had a PCB fixed, and used a laser to automatically project some dots onto the location for the next component (this was for workers assembling circuit boards by hand) but moving the board so that the component of interest is automatically centred under the microscope would be a lot more useful! Very clever if it could rotate to suit the user!

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 7 years ago

    shabaz,

     

    What a great idea (or series of ideas). The video was very good, I feel that you are quite good at capturing your ideas/explaining your process in your videos (far more comfortable than I feel anywhere near a camera).   I am going to have to start searching (amazon/ebay) for ball swivels and arms to build something like this.

     

    Some great ideas out there in response to your post:

    I was thinking that instead of concrete, you could make weighed bases using lead beads (or ball bearing/BBs/etc), filling a box (3D printed/wooden/plastic/etc) with an attachment point (1/4 - 20) affixed.

     

    I have been thinking about building an X/Y/rotate stage (not quite a robot arm) to go under my microscope to position my PCB under the field of view and positioned for the best soldering orientation (right-handed solderer).  It could run through a series of learned positions and orientations to speed up the process of building a board (sort of a pick and place but backwards idea), with a simple button press (foot pedal) to advance to the next position.

     

    Well done!

    Gene

    • Cancel
    • Vote Up +8 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to neilk

    Hi Neil,

     

    Thanks for the comments! I'm still uncomfortable and slow with creating videos, but am trying to stick with it, so I'm happy to hear that you liked it.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • 14rhb
    14rhb over 7 years ago in reply to ntewinkel

    Hi Nico,

     

    Seeing your coolant pipes has given me an idea, which might not work. He goes: use 3-4 silicon rubber tubes in parallel with the gripping components at the end. Bend it around easily into position, press the switch (ideally a foot switch) and an air compressor quickly pressurises the pipes making them act as a rigid form. The grip could perhaps also be powered by the same air source. Release the foot switch as it all relaxes again ?

     

    It would be really quick to adjust, grip and release. Downside would be the need for a power source and the noisy compressor.

     

    Of course such an idea might end up just flinging the gripped assembly/component across the workshop when all 3-4 tubes inflate with equal vigour !

     

    Rod

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>