Introduction
A few weeks ago I spotted the launch promotion of the FNIRSI DLA Logic Analyser. It’s a low-cost USB Logic Analyser offered in two versions, DLA16 and DLA32 Plus. They are currently offering the DLA16 Plus at $159 and the DLA32 Plu...
Table of Contents
Introduction
Initial usage
Setup and usage
Introduction
ngscopeclient is a free, open-source software application designed for controlling test and measurement instruments, visualizing signals, analyzing waveforms, and automatin...
Table of Contents
Introduction
What Does the Splitter Do?
Designing and Testing
Splitter Sub-System
Balun Sub-System
Impedance Transformation Sub-System
Putting It All Together
Results
Summary
Introduction
A fellow radio enthusiast was...
Introduction
I have decided to try one of the devices used for power profiling and power optimization of embedded devices. Among the devices available at a similar price point, I have narrowed my choice down to two options: the Nordic Power Profiler ...
The lab has molecular beam epitaxy (MBE), angle-resolved photoemission spectroscopy (ARPES), and time-resolved ARPES systems. (Image Credit: UCF)
Researchers are looking for new techniques to achieve faster computing. To do this, they are focusing o...
Comparing Three USB Testers Before Characterizing the FNIRSI DPS-150
Why I Did This Test
I recently added a FNIRSI FNB58 USB tester to the bench with the intention of using it during my characterization of the FNIRSI DPS-150. Before I started trusti...
A hands-on look at what it does well, where the automatic measurements can mislead you, and whether it makes sense as a first oscilloscope or portable troubleshooting tool. The tests completed in this review is not of 100% calibrated equip...
During the last test of the Si5351 clock generator, I thought that it would be nice to compare measurement results between a passive probe to an active probe. I have found one based on a well-known design with usage of the high frequency BF998 FET t...
Follow up on my road test of the Keithley Bench Digital Multimeter DMM6500.I proposed in my application to focus the review on instrument automation. In this post, the VSCode TSP Toolkit plugin. The plugin was released a few years...
Till now, I have used a self-adjusting wire stripper. It was quite good but sometimes stuttered during stripping. It didn't have an option to regulate the length of a stripped area of wire. I have decided to try something which allows me to regulate...
A while back I picked up a couple of FNIRSI instruments, a 2D15P scope and an LCR-P1 component tester. Good kit for the money, but the software is a letdown: mostly Windows-only, so on a Mac you're stuck dragging screenshot files off a USB drive by h...
{gallery}Sanwa PM300
A few years ago I looked for a replacement for my portable multimeter, the Appa iMeter 5, for which I was not fully satisfied. I have found a Sanwa PM300. I have been ...
Back in March, I was flabbergasted to be chosen as the grand prize winner for the Fun and Games competition
I mean, I was participating for the fun of it, thinking to myself "heck, if I reach second place, that'll be a good occasion to repla...
The channel isolation describes how much signal on one input channel unintentionally appears on another channel. In case when we are measuring some signal, e.g. on channel 1 and has channel 2 not connected to any signal, in an ideal scenario, there s...
Today arrived my power supply, that bought few days ago. It was a good occasion to buy almost not used device in half of current price. The device is in the condition as described by the previous owner. It still has a product seal. After disass...
Background
Today I have checked the input noise floor of the oscilloscope channel in Analog Discovery 3. By default, both oscilloscope channel inputs of the Analog Discovery 3 are not shielded. It is mentioned in this thread:
https://forum.digilent.c...
Introduction
I own a pretty old, portable PicoScope model (2000 series), which cost very little. Although I have larger desktop ‘scope options with screens, I still find that PicoScope gets used regularly. I’ve even written my own ‘...
I've desired a decent linear low-noise power supply for ages, and I think I've finally found one at a reasonable price.
(Image source: Farnell website)
It's actually been around for ages. fmilburnreviewed the 30V 5A ...
Table of Contents
Introduction
I Want to Try It, Now!
SPICE Quick Overview
Elementary Models
Pin Ordering for Component Symbols
An Entire Circuit
Choosing and Running Simulations
DC Voltages and Currents (Operating Point) Simulations
Time-Domain (...
This image combines a scanning electron microscopy (left) and a crystallographic fragment of the MXene structure, highlighting its ordered and finely tuned surface terminations. (Image Credit: B. Schröder/HZDR)
Researchers from Helmholtz-Zentru...
Introduction
I own two pairs of high-quality Moore & Wright calipers, which offer several advantages: an excellent LCD screen, soft-press buttons, and straightforward operation. However, there are some drawbacks. The battery compartment slide cov...
Michael Stoops submitted pull requests to make a set of USB parameters configurable in your CMake file.
What USB IDs can be configured?
USB_VID
USB_PID
USB_MANUFACTURER
USB_PRODUCT
USB_SERIALNUMBER
FW_VER_BCD
FW_VER_STR
Before&n...
Introduction
I recently bought a new laptop to replace an ancient one, and this time decided to put more thought into how I organized things.
A problem for me is that I tend to install a lot of software tools and integrated development environments (...