Test & Tools
  • Technologies
  • More
Test & Tools
Blog DC Voltage Measurement Accuracy: AD584KH voltage reference
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 20 Jun 2023 8:47 PM Date Created
  • Views 5226 views
  • Likes 14 likes
  • Comments 37 comments
  • dmm6500
  • reference
  • keithley
  • AD584
Related
Recommended

DC Voltage Measurement Accuracy: AD584KH voltage reference

Jan Cumps
Jan Cumps
20 Jun 2023
DC Voltage Measurement Accuracy: AD584KH voltage reference

Follow up on  DC Voltage Measurement Accuracy: Measuring DC voltage with high accuracy on a DMM6500 . 
I bought a little voltage reference based on Analog Device's AD584 .

image

The reference is the AD584KH. The kit supports the 4 programmable reference values. It comes with a label showing measurements on a HP 3458A

image

image

image source: analog devices datasheet

Calibration values (25° / 49% humidity):

  • 2.49974
  • 5.00203
  • 7.50113
  • 10.00277

Calibrated by http://www.haoqielec.com/wap/en/aboutus.html

Checking Keithley DMM6500

I let the reference and DMM warm up for an hour. Room temperature was 26°. Humidity unknown

image

I used Keithley's TSP script "Measuring DC voltage with high accuracy". I used that in the previous post too.
The Test Script Builder log gives a higher resolution than the 6500 display.
I let the reference settle for 5 minutes on each value before running the script and getting the measurement

CAL (HP 3458A DMM6500 round
2.49974 2.4997806153 2.49978
5.00203 5.0021082424 5.00211
7.50113 7.5012037198 7.50120
10.00277 10.002870735 10.00287

Thoughts and remarks? Post them in the comments

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 3 years ago in reply to ggabe +2
    Hopefully these photos can be zoomed up without the content system compression causing issues: The marking is A1 HB , or possibly A1sHB , and it looks like it is Si2301 (P-ch MOSFET) . I have some…
  • ggabe
    ggabe over 3 years ago in reply to Jan Cumps +1
    Could it be a ground current? What if you battery power and also connect the USB ground?
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to scottiebabe

    It only serves to switch between the 4 output values.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago in reply to Jan Cumps

    If it was common-mode noise or ground loop noise, you would only need to touch the usb plug shell to the connector shell (just connect the grounds) to observe the disturbance.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago in reply to Jan Cumps

    image

    Is that soic-16 a shift register then? Neat, but the output excursion is terrifying Scream cat lol

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to scottiebabe

    There is no MCU. It's the output of the AD584 Scream

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to ggabe

    > What if you battery power and  also connect the USB ground?

    Can't. When I do that, the circuit tries to charge the battery and I could not find a chargeable of this type.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>