Test & Tools
  • Technologies
  • More
Test & Tools
Blog Trying Out the Rossmann Flux
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 8 Feb 2019 12:41 PM Date Created
  • Views 5719 views
  • Likes 11 likes
  • Comments 15 comments
  • flux
Related
Recommended

Trying Out the Rossmann Flux

Jan Cumps
Jan Cumps
8 Feb 2019

One of the things that jump out in Louis Rossmann's videos is the type of flux he uses (and the amount image).

The fluxes I have at home are liquid, and that works well when building new PCBs. The Amtech flux I'm testing here is a jelly when applied and becomes fluid when hot. This may be helpful when reworking surface mount ICs, where my flux is gone by the time I'm halfway reworking them.

image

 

What I'm hoping to get out of this is to improve my success rate when reworking QFN packages and the likes.

I'm not the fastest guy on earth when dealing with these types of components.

 

What's included?

 

The flux is AMTECH's NC-559-V2-TF. It comes in a syringe. A plunger and dispense needle are optional.

There's 10 ml in the container. That should be plenty for me. I expect that the shelf life of one year will expire before I've consumed all.

I got one from a fresh batch. It's manufactured in the same month that I placed my order.

 

Although the label says that it's a lead-free soldering material (technically correct, because there's no lead in the flux), it's not compatible with leaded solder.

There is a lead-free variant (VS-213-A-TF).

 

The flux isn't corrosive and can be left on the board, but the manufacturer advises against that.

It makes the board more prone to contamination. It can result in increased voltage leakage for sensitive designs and can become a moisture trap.

 

I'll try it out soon and report back on the experience.

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 7 years ago in reply to jw0752 +4
    It’s almost as baldengineer ’s experience with ChipQuick’s flux. The only thing it doesn’t do is form a bubble and boil. It forms a fluid film that stays in place. I just retried reflowing a TQFN package…
  • neilk
    neilk over 7 years ago in reply to Jan Cumps +3
    I'm still using the same spool of leaded solder I bought over 20 years ago. This shows 2 things: How inactive I was until I joined this forum That I mostly software - hardware (ie soldering) only when…
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to neilk +3
    This is what's left from the last one I bought when at school (must be a roll from 85 or early 86): I switched to lead free, not for the environment as primary reason, but because it's a required skill…
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to neilk

    This is what's left from the last one I bought when at school (must be a roll from 85 or early 86):

    image

     

    I switched to lead free, not for the environment as primary reason, but because it's a required skill in the industry.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • neilk
    neilk over 7 years ago in reply to Jan Cumps

    I'm still using the same spool of leaded solder I bought over 20 years ago. This shows 2 things:

     

    1. How inactive I was until I joined this forum
    2. That I mostly software - hardware (ie soldering) only when I have no other choice!

     

    Neil

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to jw0752

    It’s almost as baldengineer’s experience with ChipQuick’s flux. The only thing it doesn’t do is form a bubble and boil. It forms a fluid film that stays in place.

     

    I just retried reflowing a TQFN package I did a few weeks ago (remove and place back) with hot air and that worked well.

    I put flux, tinned the pads with an iron, put back the IC and reflowed with hot air.

     

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 7 years ago

    I am eager to look over your shoulder and learn from your experiments.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • baldengineer
    baldengineer over 7 years ago

    Do you have any experience with ChipQuik SMD291? I am curious how the Amtech compares to ChipQuik. (Is there any significant difference?)

     

    I've been working with SMD291 recently and found the jelly-like viscosity to be a huge help. It's so much easier to get flux into tight pitched ICs. While it works fine for pencil soldering, I found the way its surface tension holds a bubble shape means it starts boiling before the tip comes in contact with metal. I'm not sure if that is good or bad, but it is different from my experience with liquid flux.

     

    For surface mount parts, it works fantastic. Even with liberal usage, I don't feel like my syringe is moving at all.

     

    I've also found it is fantastic to soak into solder wick for de-soldering tasks. Compared to liquid flux, the jelly soaks into the weave so much better.

     

    Anyway, I'm very curious to see your experience and maybe compare notes. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>