Wearable Technology
  • Technologies
  • More
Wearable Technology
Blog Christmas Hat: Connections
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wearable Technology to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: brenyc13
  • Date Created: 22 Nov 2014 12:53 PM Date Created
  • Views 1224 views
  • Likes 1 like
  • Comments 4 comments
  • wearable_technology
  • christmas_hat
  • haturday
Related
Recommended

Christmas Hat: Connections

brenyc13
brenyc13
22 Nov 2014

A brief post in which I hook everything up and see if it works.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

NeoPixel Strip

Strip 5v >> Flora VBatt

Strip Din >> Flora D6

Strip GND >> Flora GND

 

I’d sketched out how everything fit together in my last post, so all I needed to do was break out the alligator clips and my cute little breadboard and follow my plan. I first connected the 1.5-meter Neopixel strip to the Flora, with alligator clips and ran the Neopixel strip test. Miraculously, it worked on the first go.



image

 

Through-hole NeoPixels

LED Din >>Flora D9

LED 5v >>Flora VBatt and next LED

LED GND >> Flora GND and next LED

LED Dout >> next LED

 

I disconnected those alligator clips from the Flora and placed one of the 5mm through-hole NeoPixels in my breadboard. I cut and placed small bits of wire to correctly power and connect the LED to the Flora. Then I found the Punk Collar code and changed the pin number to pin 9 and uploaded it to the Flora. The light changed color beautifully. Then I placed the remaining four through-hole NeoPixels in the breadboard so that each Data-Out pin was column-buddies with the Data-In pin of the following LED, and used more little pieces of wire to connect each to power and ground. I ran the Neopixel Tiara code again and they worked.

 

image

 

Temp Sensor

Sensor Vin >> Flora 3.3v

Sensor Dout >> Flora D10

Sensor GND >> Flora GND

 

I disconnected the LEDs at the Flora end and placed my temperature sensor on the opposite side of the breadboard, using more wires to connect it to the Flora. Then I uploaded the example Simple Thermometer code and opened the serial port to find that the room was a sweltering 138 degrees fahrenheit. That didn’t seem quite right. So I read over the Temp Sensor overview and realized that it was calibrated to receive 5 volts of electricity and I was only giving it 3.3 volts. I changed the calculation to compensate, re-uploaded the code, re-opened the serial port, and all was well. A perfectly reasonable 70 degrees.

 

image

 

So everything is functioning. Next, I’ll start writing code and using the NeoPixels and sensor together. Hopefully it keeps working!


  • Sign in to reply
Parents
  • mcb1
    mcb1 over 12 years ago

    Nice work.

    I didn't realise the neo-pixels were available in that form ... very handy for my next project.

     

    Thanks

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mcb1
    mcb1 over 12 years ago

    Nice work.

    I didn't realise the neo-pixels were available in that form ... very handy for my next project.

     

    Thanks

    Mark