Wearable Technology
  • Technologies
  • More
Wearable Technology
Forum 3D Printed Dress...I would totally wear this....
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wearable Technology to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 53 subscribers
  • Views 4677 views
  • Users 0 members are here
  • 3d
  • 3d_printing
  • Wearables
  • 3d_printed
Related

3D Printed Dress...I would totally wear this....

summerella
summerella over 11 years ago

Wearables are sometimes thought of as still a bit abstract, but here is something I would wear now...if it wasn't $3,000 USD. Although made of plastic, it seems to have a great flow and more fabric-like movement.

 

Do you think we will move towards 3D printed clothing (clothes could be customized and cut exactly to fit), or will we continue with traditional fabric production and tailoring?

 

This 3D printed plastic dress flows like fabric - CNN.com

image

"The design studio Nervous System has created a novel process that allows a 3-D printed dress to move and sway like real fabric. The bespoke software behind it, called Kinematics, combines origami techniques with novel approaches to 3-D printing, pushing the technology's limits.

Instead of pinning fabric to a dress form, a Kinematics garment starts as a 3-D model in a CAD program. Kinematics breaks the model down into tessellated, triangular segments of varying sizes. Designers can control the size, placement, and quantity of the triangles in a Javascript-based design tool and preview how the changes will impact the polygonal pinafore. Once the designer is satisfied, algorithms add hinges to the triangles uniting the garment into a single piece and compress the design into the smallest possible shape to optimise the printing process, often reducing the volume by 85 percent."

 

Read the rest of this WIRED article on This 3D printed plastic dress flows like fabric - CNN.com

  • Sign in to reply
  • Cancel

Top Replies

  • summerella
    summerella over 11 years ago +2
    Interesting comments guys, I appreciate them!! I agree 3D printed clothes are not practical in terms of time, cost, or efficiency...YET. Give it some time though. It will open up so many possibilities…
  • michaelkellett
    michaelkellett over 11 years ago in reply to summerella +2
    Shoes are more likely in the short term - it might be practical to 3d print a pair of custom frames (for want of a better word) and then cover them with cosmetic material for appearance, at a much lower…
  • shabaz
    shabaz over 11 years ago +1
    Hi Summer, It's impressive that they have a way to produce such a large, flexible item : ) I think many things will move towards a version of fabrication that doesn't rely on traditional labour or tailoring…
Parents
  • shabaz
    shabaz over 11 years ago

    Hi Summer,

     

    It's impressive that they have a way to produce such a large, flexible item : ) I think many things will move towards a version of fabrication that doesn't rely on traditional labour or tailoring as you suggest. This would allow people to have more custom, unique items, and also produced locally, where skills and labour may not exist to create in traditional ways. When the order is placed, that unique item can be manufactured and supplied.


    As I understand, already car manufacturers have some items (e.g. vehicle interior trim) located in different places in the world, so that once the car is shipped from the point of manufacture, the remainder customisation occurs much closer to the customer.

     

    However, how long it will take I'm not sure : ) I thought 3D printers were in their infancy apart from creating prototypes, yet some results (such as this dress) show that maybe things are further ahead that I thought!


    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 11 years ago

    Hi Summer,

     

    It's impressive that they have a way to produce such a large, flexible item : ) I think many things will move towards a version of fabrication that doesn't rely on traditional labour or tailoring as you suggest. This would allow people to have more custom, unique items, and also produced locally, where skills and labour may not exist to create in traditional ways. When the order is placed, that unique item can be manufactured and supplied.


    As I understand, already car manufacturers have some items (e.g. vehicle interior trim) located in different places in the world, so that once the car is shipped from the point of manufacture, the remainder customisation occurs much closer to the customer.

     

    However, how long it will take I'm not sure : ) I thought 3D printers were in their infancy apart from creating prototypes, yet some results (such as this dress) show that maybe things are further ahead that I thought!


    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • michaelkellett
    michaelkellett over 11 years ago in reply to shabaz

    It's an interesting (and clever) experiment but miles away from making anything useful or efficiently.

    Although 3D printing is often touted as an additive technique (unlike machining form solid) the process used here generated a staggering amount of waste - and it took 2 DAYS to print !

    Classical techniques like weaving cutting and stitching are much more efficient - in both machine time and material and energy use.

    3D printing has a very long way to go and my bet is that it will be a niche thing - I don't expect to see it replace classical mass production techniques any time soon.

     

    The 'dress' is like so many 3D printed artifacts - hugely compromised to suit the process - how many uses are there for clothes with great big holes in them and plastic parts with loads of little ridges ?

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to michaelkellett

    Ah, I didn't realize how excessive the waste material was. I agree, it won't necessarily be 3D printers (at least not like what they are now). And it is definitely a long way to go - I can't imagine seeing moulding machines, CNC mills etc being replaced for a long time for the reasons you mention (speed, energy, waste, etc).

    I wonder if it will occur 50 years from now.. I can see it being attractive at some point when/if technology improves on speed, energy and so on, for businesses to be able to create arbitrary rigid objects (tables, chairs etc) locally and have them delivered a short distance, but perhaps those 3D printers will be industrial machines taking bars of material or something. Or we might have ruined the world by then, and time to go back to basics. Good thing I can still use a saw.. : )

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • gadget.iom
    gadget.iom over 11 years ago in reply to michaelkellett

    Have just watched the video, I can't work out where the wastage is in the process.

    It's an excellent proof of concept and if manufacturing technology can improve in the future it might be a viable solution.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 11 years ago in reply to shabaz

    Probably printing them out as little chain mail items. They would initially be stuck together but if they were only joined by a little bit of material you probably could shake and break them free from each other so they become more like mail.

     

    Failing that it could be one of the new flexible materials in which case there is no reason to make it out of holes other than to show off as much as the model as possible image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 11 years ago in reply to gadget.iom

    3D printing is really only useful for low volume an prototype work at the moment it's simply too slow for  high volume low profit items which really need the old school tooling/ machining methods.

     

    One thing which is holding up the wide spread use of them is that they are slow expensive but more critically require an element of talent to design and create the object .

    Most people just want to go to the shop and buy it!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • gadget.iom
    gadget.iom over 11 years ago in reply to Problemchild

    Very true. I'm just trying to work out where a staggering amount of waste was being produced. I know that the video shortened sequences and skipped steps.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 11 years ago in reply to gadget.iom

    Picture 6 at http://edition.cnn.com/2014/12/17/tech/innovation/3d-printed-plastic-dress/index.html?hpt=hp_bn5

     

    She isn't wearing that "boulder sized" lump of plastic. I assume it's either support structures or that they used one of the dust sintering processes.

     

    It may be possible to re-cycle plastic dust but I know that when you do it with metal that even the unused dust need reprocessing.

     

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gadget.iom
    gadget.iom over 11 years ago in reply to michaelkellett

    I believe that boulder is the finished dress buried in the unbound dust material. The dust is blasted away and can typically be reused.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 11 years ago in reply to gadget.iom

    The dust is reusable, This really depends on the technology.

    A lot of these are actually Gypsum dust and is specified as recyclable not least that in many designs only about 5% of the material dispensed is in the finished product so there is a big need for this.

     

    This "plastic" dress may actually be a gypsum one because they use "plastic" binders to hold the parts together so this may be where the "plastic" comes from!