Wireless
  • Technologies
  • More
Wireless
Blog Do I Need a New Router when I Upgrade to Wi-Fi 6?
  • Blog
  • Forum
  • Documents
  • Polls
  • Quiz
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wireless to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dychen
  • Date Created: 22 Dec 2022 6:14 PM Date Created
  • Views 2273 views
  • Likes 10 likes
  • Comments 2 comments
  • 802.11
  • wi-fi6
  • wi-fi
  • network
  • wi-fi 6
  • wireless
  • router
  • ieee
Related
Recommended

Do I Need a New Router when I Upgrade to Wi-Fi 6?

dychen
dychen
22 Dec 2022

Wi-Fi 6 (aka IEEE 802.11ax) is the latest iteration of the Wi-Fi network protocol. It is a significant upgrade over its predecessor 802.11ac (retroactively renamed Wi-Fi 5). This advanced network protocol allows for faster connection speeds with improved power efficiency and performance. Wi-Fi 6 allows access points (AP) to support more clients in dense environments, and offers a superior experience for users of typical wireless LAN networks. It also uses Target Wake Time (TWT) that schedules wake times to improve client battery life. In this article, we will discuss Wi-Fi 6 capabilities and router compatibility with older generation routers.

Wi-Fi Timeline

The Institute of Electrical and Electronic Engineers (IEEE) develops standards for computer networking and provides continuing innovations, maintenance, and amendments services for these standards. Wi-Fi is the colloquial term for Wireless Local Area Network (WLAN) technology and is a brand name used to market the 802.11 standards.

The 802.11 working group is responsible for writing and developing new WLAN standards. The working group oversees the work done by all the 802.11 "task groups." Each group is assigned a letter from the alphabet, and the term “802.11 alphabet soup” designates all the amendments edited by the multiple 802.11 task groups. Each amendment aims to enhance the 802.11 technology, with many enhancements vying for higher data rates and faster speeds (see Table 1).

Year

Amendment

Data rates

2.4 GHz

5GHz

RF technology

Radios

1997

802.11 legacy

1 and 2 Mbps

ü

 

DHSS and FHSS

SISO

1999

802.11a

6-54 Mbps

 

ü

OFDM

SISO

1999

802.11b

1,2,5.5 and 11 Mbps

ü

 

HR - DSSS

SISO

2003

802.11g

6 - 54 Mbps

ü

 

OFDM

SISO

2009

802.11n

up to 600 Mbps

ü

ü

OFDM

MIMO

2013

802.11ac

up to 6.93 Gbps

 

ü

OFDM

MU - MIMO

Table 1: 802.11 technology Timeline

The term multi-user (MU) implies that the transmissions between an AP and multiple clients can co-occur, depending on the supported technology.

What is Wi-Fi 6 (802.11ax)?

802.11ax is an IEEE draft amendment that enables high-efficiency operations in frequency bands between 1 and 6 GHz. It is a modified version of the 802.11 Physical (PHY) layer and the Medium Access Control (MAC) sublayer. The 802.11ax is also called High-Efficiency Wireless (HEW).

The Wi-Fi Alliance, a non-profit organization advocating the use of WLAN, has recently adopted a new generational naming convention for Wi-Fi technologies. The new naming scheme will help users differentiate between the various Wi-Fi technologies. It uses a numerical approach to identify Wi-Fi generations, where the numbers correspond to essential advancements. The 802.11ax technology is known by the generational name Wi-Fi 6 as it is a significant transition from previous versions of 802.11 technology. Figure 1 shows the new naming convention.

Generations of Wi-Fi

Figure 1: Generations of Wi-Fi

Wi-Fi 6 — More than just speeds and inputs

A Wi-Fi 6 implementation is highly configurable due to channel bandwidth, spatial streams, and multi-user signaling mechanisms. The lower end of the throughput range targets small handheld devices such as smartphones. The middle of the throughput range aims towards laptops, and the highest end of the throughput range targets outdoor and specialized applications where the device density is much lower when compared to indoors.

Wi-Fi 6 technology focuses on better use of the existing radio frequency medium. The goal is more efficient and improved 802.11 traffic management. Another notable Wi-Fi 6 change is that an access point (AP) can control the medium, and supervise downlink and uplink transmissions to many client radios. Besides these multi-user efficiency upgrades, Wi-Fi 6 (802.11ax) radios are backwards compatible with the 802.11/a/b/g/n/ac radios.

Table 2 shows examples of Wi-Fi 4, Wi-Fi 5, and Wi-Fi 6/6E configurations for targeting specific devices or applications.

 

Wi-Fi 4

Wi-Fi 5

Wi-Fi 6

Wi-Fi 6E

Frequency bands

2.4 GHz and 5GHz

5GHz only

2.4 GHz, 5 GHz

6Ghz

Channel size (MHz)

20, 40

20, 40, 80, 80+ 80, and 160

20, 40, 80, 80+ 80, and 160

20, 40, 80, 80+ 80, and 160

Frequency multiplexing

OFDM

OFDM

OFDM and OFDMA

OFDM and OFDMA

Modulation

Binary Phase-Shift Keying(BPSK), Quadrature Phase Shift-Keying(QPSK), 16-QAM(Quadrature Amplitude Modulation), 64-QAM

BPSK, QPSK, 16-QAM, 64-QAM, 256-QAM

BPSK, QPSK, 16-QAM, 64-QAM, 256-QAM, 1024 QAM

BPSK, QPSK, 16-QAM, 64-QAM, 256-QAM, 1024 QAM

Max Data rate

600 Mbps

Up to 6.93Gbps

9.6Gbps(1.5Gbps per device)

9.6Gbps( 2.3Gbps per device)

Table 2: Wi-Fi 4, 5, 6, and 6E comparison

Extending Wi-Fi 6 into 6 GHz

The industry identifies Wi-Fi devices operating at 6 GHz as Wi-Fi 6E. An important differentiator is the non-requirement for backward compatibility when using the 6 GHz frequency band for 802.11ax technology. Protection mechanisms are unnecessary as 802.11a/b/g/n/ac radios operate only on the 2.4 GHz or 5 GHz band. 

Is My Old Router Compatible with WI-FI6/6E?

Routers that are older than approximately three years will not support Wi-Fi 6, and must be upgraded. WLAN vendors already sell Wi-Fi 6E APs in many different form factors. Wi-Fi 6 routers are compatible with devices dating back to the early 2000s, and these devices have radios for all three bands (2.4, 5, and 6 GHz). However, only the new Wi-Fi 6E client devices with 6 GHz radios can communicate with the 6 GHz radio in a Wi-Fi 6E AP. An older dual-frequency (2.4 and 5 GHz) smartphone communicates solely with the 2.4 or 5 GHz radio in a tri-band Wi-Fi 6E AP.

Most devices slated to sell in the next few years—including PCs, smartphones, tablets, and TVs—will be Wi-Fi 6-certified.

  • Sign in to reply
Parents
  • Andrew J
    Andrew J over 3 years ago

    Wifi 6E routers are eye-wateringly expensive at the moment, particularly if you opt for a mesh router.  I was looking at a new router recently because it was put to me that the Internet problems I was experiencing was because mine was faulty.  You go for the latest model right to future-proof?  Of course you do, and the latest Orbi 6E mesh router with 1 AP was around £1500!!!  An Orbi Wifi 6 router and AP was around £700 so still way too expensive.  At that point I decided I was right and it wasn't a router problem and OpenReach/Plusnet just needed to pull their collective fingers out.

    Some good information in this post.  Small households like mine (me and my wife) don't really come up against bandwidth or speed issues; I could imagine a house with 4 teenagers would be a lot different.  One of my in-laws has 3 boys all of an XBox/Playstation age and all like to play on-line.

    A lot of mesh routers are sold as tri-band at the moment: 2.4, 5, and backhaul for the APs.  Does that mean that to get the best out of a Wifi 6E deployment you'd want a quad-band? 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Fred27
    Fred27 over 3 years ago in reply to Andrew J

    What about the Google Nest Wifi Pro? £190 for one or £380 for a 3-pack mesh.

    https://store.google.com/gb/product/nest_wifi_pro?hl=en-GB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Fred27
    Fred27 over 3 years ago in reply to Andrew J

    What about the Google Nest Wifi Pro? £190 for one or £380 for a 3-pack mesh.

    https://store.google.com/gb/product/nest_wifi_pro?hl=en-GB