Wireless
  • Technologies
  • More
Wireless
Blog How We Lost Flight MH370
  • Blog
  • Forum
  • Documents
  • Polls
  • Quiz
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wireless to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: kas.lewis
  • Date Created: 17 Mar 2014 8:54 PM Date Created
  • Views 2863 views
  • Likes 3 likes
  • Comments 8 comments
Related
Recommended

How We Lost Flight MH370

kas.lewis
kas.lewis
17 Mar 2014

As we go into another day wondering where Malaysian Airlines MH370 is, the biggest question is: how does such a big airplane vanish with no apparent trace? But first we need to understand how airplanes are tracked today.

 

9M-MRC-Malaysia-Airlines-Boeing-777-200_PlanespottersNet_286025.jpg

 

The 777 is one of Boeing’s most advanced aircraft with some of the most up-to-date communication equipment on board. There are four primary methods of communication with an airplane. The first is the standard method of radio communication. This is where the pilot informs air traffic control of his position and altitude verbally.

 

The second method of communication is via radar, in this category there are two types. The first is primary radar, this is simply the radio reflection of the airplane (sort of like the way a flashlight lights up an object in a dark room). While the commercial version of this first type of radar may tell you how far an airplane is from the ground station, it does not convey altitude or airspeed, for this secondary radar is used. Secondary radar sends a signal to the airplane asking it for more information. Since the direction from which the signal was sent is known, the general direction of where the airplane is is also known. When the airplane’s onboard transponder sends back information (altitude, airspeed, etc) then the complete picture is displayed on the air traffic controller screen (ATC): position, altitude, and airspeed.

spaceout.gifsonar-scope-7392911.jpg

The third method of communication is starting to become more mainstream and will become required by the FAA by 2020. This is called Automatic Dependent Surveillance-Broadcast (ADS-B). With ADS-B, more information is transmitted back to the ground station and does not depend on ground-based stations for receiving/transmitting data. It is connected via satellite to any necessary ground station. The benefits of this are obvious when we look at flight MH370 and a bit further back at Air France 447. With AF477 it was not known that the flight had a catastrophic event until at least 2 hours later, when it was supposed to be flying over Senegal. The reason for this is that flights routinely “vanish” from their digital tracks. When a flight leaves a radar-controlled space, say, flying across the Atlantic where there is no real-time radar tracking, the flight’s last known position, airspeed, and planned flight path are used to predict its progression along its route. When the flight arrives again at a radar controlled zone it is supposed to check in. In AF477’s case, when the first ATC failed to get an acknowledgment from the flight’s pilots, he assumed they either did not hear him or they were busy. It was only when a later ATC in Senegal looked further into the matter (when he, too, failed to get an acknowledgment) that it was discovered that AF477 had had a catastrophic event. This is something the ADS-B would remedy. Even with a transmission rate of once per 30 minutes, it would still offer far greater accuracy to determine where a flight truly is.

 

The last method of communication between the ground and an aircraft is something called Aircraft Communications Addressing and Reporting System (ACARS). ACARS is a text-based system that allows the airplane and pilots to send information to the aircraft manufacture and airlines headquarters to report anything from routine maintenance issues to possible weather alerts along the flight path. The ACARS can also be used as a kind of “are you alive” signal since it apparently can not be turned off. In the MH370’s case it is this signal that has led investigators to believe that the plane flew for more than 5 hours after all other forms of flight tracking were turned off since this signal was repeatedly received hourly between 4 and 6 times after the flight vanished.

 

With all these communication systems in place one would think that it would be difficult for a plane to completely disappear. According to the current assumed flight path, it is thought that the plane flew back over Malaysia and possibly over mainland Asia. So how does a plane just disappear? Even if all onboard systems could be turned off, couldn’t radar track it since the plane was apparently flying over land and in some cases even through militarized areas?

 

Let’s start with the onboard communication devices: the transponder, the radio and the ADS-B. These can all be turned off, except for the ACARS. Far from being bad design, this is a necessary safety requirement. In the event of a short circuit that could lead to a fire all systems on board need to have the ability to be shut down. So if the onboard systems were turned off why did no one notice? The answer to this is based on how flights are tracked when out of range of radar. Above it was explained that when a flight leaves a radar-controlled zone it is tracked virtually, that its last known position, airspeed, altitude and flight plan are used to predict where it is at any given moment. This projection is used until the aircraft arrives back in a radar-controlled zone.

 

image

 

OK, so all major tracking systems are turned off,. But why can't they see the flight on radar? The answer here is one that might be a bit surprising. In civilian air traffic control towers, most controllers turn off the primary radar reflection to remove clutter. Clutter like: birds, clouds--  anything that the radar picks up but may not necessarily be an airplane. So to get a clearer picture of what is really important, air traffic controllers turn off the primary image and leave the secondary image, which displays all confirmed flights in the area. This does not, however, mean that military installations in the area won't see you. But in Malaysia, India and other countries in the area, military radar is only turned on when there is a good reason, such as a perceived threat. There is also the possibility that someone with knowledge could fly around or under military radar. The aircraft would need to fly under 5000 feet to pull this off-- no simple task, but also not impossible.

 

So now that we have evaded both civilian and military radar operators, what do we do with the plane? This is one of the bigger issues with this theory, but even this is not impossible to speculate about. In an emergency, the Boeing 777 has the ability to land on a relatively small runway that may or may not be paved. It has been stated that even a well-packed dirt runway could potentially be used. For someone that has worked out how to get a plane this far, getting it on the ground would hardly be a difficult task.

 

The real frightening question is with a plane full of people on a remote air strip somewere, what do you do with these people? I hope and pray that nothing barbaric or inhumane took place.

 

Now that we have a potential scenario of how a plane just vanishes, how do investigators have any idea where the plane may be? This is where the ACARS has proven useful. It reports back to the plane manufacturer on routine maintenance issues as well as engine operating conditions. This information is used to monitor the health of an aircraft even before it is brought in for inspection. Although this is a paid service and not all airlines use it (Malaysian Airlines apparently does not pay for this service) it is still a useful system. It’s the same reason many cell phones work both in their immediate service area, and also in new areas: phones respond to requests for information even if the request comes from a different service provider. In the case of the ACARS the system sends out a ping to all radios even if that particular plane is not subscribed to the service. The onboard system then responds with an acknowledgement of the ping. It is this information that investigators have used to give a radius of where the flight may have ended up. This is calculated by taking how long it took from the time the signal was sent out to the time the acknowledgment was received, half of this time is the distance to the airplane. The limitation with this is that it still gives a very large search area-- tens of thousands of miles-- even if remaining flight time is taken into account based on available fuel. We’re still talking about a vast area.

 

image

 

So how can we use this information to prevent a plane from vanishing in future? I believe the ACARS system is the answer to preventing planes from vanishing. When a plane responds to a remote ping, it must reply in a standard format. Adding a few more fields to the message would add very little overhead and cost to the existing system, and could provide GPS location information of the flight. This would narrow a search from hundreds of thousands of square miles down to hundreds of square miles. In the case of flight MH370, it would have told us where the plane had been over its last 5 hours of flight, which would have significantly reduced its current search radius.

 

What do you think? I’d love to know what you think could help improve aircraft location technology. Post your thoughts below in the comments.




 





Tweet

Follow @Kazzzzzzzzzzz

Follow Kas' blog
  • Sign in to reply
Parents
  • rew
    rew over 12 years ago

    Hey DAB,

    Suppose your wife says she's going to drive over to her mother at 4 hours away. She could crash  a few miles away, and her mother might not raise the alarm until she is an hour late, so you would be "not knowing" of a problem for five hours! Can you force everybody to install GPS tracking and satellite communications systems on all the cars just to be able to inform you of a crash involving your wife?

     

    It is always a cost-benefit analysis.

     

    A different example: Modern Flight Data Recorders (FDRs) record hundreds of parameters of the plane. When a plane crashes you'll always find that one that could have made the investigation easier is missing. For example, the crash of Asiana 214 at San Francisco: The autothrottle turned off 80 seconds before the crash. The reason why was not recorded. Recording why autothrottle systems turn off would help that investigation. So we could force all air planes in the world to upgrade their FDR. Cost to the industry: Lots. Benefit: not a lot. Result: the NTSB has a riddle to solve in this case and in future cases.

     

    REAL safety measures are more important by the way. A measure like "improved FDR" will make the investigation easier, but it won't prevent accidents from happening. OK, in the long run a "solved" accident might  lead to measures that prevent future accidents from then on. I just read today that Senators are pushing for immediate and  mandatory installation of video recording equipment in trains, because the NTSB has said that it would've made their investigation easier. Immediate compliance for safety reasons!

     

    Not a good argument. We don't have those kinds of accidents on a daily basis. It is not that we must prevent them NOW because next month we'll have had 20 more accidents killing hundreds of people. The system is acceptably safe and if an investigation or a search takes a long time, during that time there are always "it would have been be nice if we'd had XXX installed" arguments.

     

    If there already is a communications system via satellites, and if it would not cost too much bandwidth it would indeed be nice to send the "current position" through that system. For planes not flying, once an hour, for planes flying maybe once every 15 minutes. That would seriously narrow things down.

     

    The bandwidth issue is IMHO a possible problem. I'm not aware of any of the numbers, so I can't even do a ballpark calculation. But there is a significant bitrate of data if ALL planes worldwide would continuously report their position. To buy such bandwidth "via satellite" could be very costly.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 12 years ago in reply to rew

    Hi Roger,

     

    You are mixing apples and oranges.

    If my wife crashes the car, there are hundreds of people nearby who can get her assistance long before I need to be notified.

    We are talking about aircraft flying over remote areas of the world where a crash could go unnoticed for hours/days.

    I understand the cost benefit issues, but we are talking about a 100 Million dollar aircraft and 297 people.  The whole issue about air service is that they endeavor to transport you from point A to point B safely and on time.  Anything that impacts either of those two issues should be known to the airline within minutes.

     

    Monitoring aircraft is already done, there is just no procedures for automated tracking.  It would be very easy to install a twitter like update from the aircraft whenever an unexpected event occurs.

    You can easily justify the maintenance monitoring at a minimum, which is why the engines continued to attempt to send operation data at regular intervals.

    Having someone shut down vital aircraft systems should have immediately sent an alarm throughout the flight path for an alert of a potential problem on the aircraft.

     

    Cost is not the issue.  Responding to emergency events requires quick responses.  Any EMT will tell you, minutes count.  So the earliest you can alert everyone that their services might be needed, the better they can prepare.  Plus the lessons of aircraft hijacking should make it standard procedure to monitor all aircraft all of the time.  There is a very critical need to know if an aircraft is doing something it should not.

     

    This is not a nice to have issue.  We all have a need to know if an rogue aircraft is in the sky heading to our airspace.  To pretend otherwise ensures that people will die when we could have prevented it.

    Ask the families of the passengers.  How much extra would they have paid to have the aircraft monitored.

     

    As I said earlier, we have the technology, we have the network applications ready to do the monitoring, all we need is a procedure to implement the safety system.

     

    Besides, you could easily sell and app for smart phones that would keep everyone up to date on an aircraft of interest.

    If your wife was in an aircraft coming home and you needed to pick her up, wouldn't you want to know that she was going to be hours late due to a problem with the aircraft?

    A simple phone call could greatly brighten your world.

     

    In the US, we have automated tracking of most of our rail lines.  If we can track that many rail cars, we can easily track the hundreds of aircraft in the air at any point in time.

     

    I am not trying to invent a new government agency.  I am just saying that we can and should keep track of aircraft.  We all have a need to know if one is in trouble or being used for bad things.

     

    Just my opinion,

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to DAB

    where a crash could go unnoticed for hours/days.

    Unfortunately we have experieced a few car crashes where this has also occurred, despite extensive searching.

     

    Besides, you could easily sell and app for smart phones that would keep everyone up to date on an aircraft of interest.

    Already have that its called FlightExplorer, but like the other systems relies on the data sent out by the aircraft.

    The data is delayed to prevent other issues and together with ADSB gives the ability to see the arrival time.

    I always use the information on the Airport website to check on flight arrivals.

     

     

    While it may take a long time to determine the true cause of this, we need to be open minded to the fact it may be some other event that has caused it.

     

     

    While I have no issues with items that do increase safety, having a tracking system that is independant of existing survellance systems at an ATC location, is NOT going to improve the situation, so there is a cost.

    We also need to remember that there is a maintenance cost to every nut and bolt on an aircraft, so the initial purchase cost is only one part of it.

    Often the maintenance cost is higher than the iniitial purchase.

     

    I've yet to be convinced how extra tracking would have prevented this (or any future) from happening.

     

     

    Cheers

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mcb1
    mcb1 over 12 years ago in reply to DAB

    where a crash could go unnoticed for hours/days.

    Unfortunately we have experieced a few car crashes where this has also occurred, despite extensive searching.

     

    Besides, you could easily sell and app for smart phones that would keep everyone up to date on an aircraft of interest.

    Already have that its called FlightExplorer, but like the other systems relies on the data sent out by the aircraft.

    The data is delayed to prevent other issues and together with ADSB gives the ability to see the arrival time.

    I always use the information on the Airport website to check on flight arrivals.

     

     

    While it may take a long time to determine the true cause of this, we need to be open minded to the fact it may be some other event that has caused it.

     

     

    While I have no issues with items that do increase safety, having a tracking system that is independant of existing survellance systems at an ATC location, is NOT going to improve the situation, so there is a cost.

    We also need to remember that there is a maintenance cost to every nut and bolt on an aircraft, so the initial purchase cost is only one part of it.

    Often the maintenance cost is higher than the iniitial purchase.

     

    I've yet to be convinced how extra tracking would have prevented this (or any future) from happening.

     

     

    Cheers

    Mark