Wireless
  • Technologies
  • More
Wireless
Blog Next-gen WLAN: What you need to know about 802.11ac and why 2.5 Gbps is critically important
  • Blog
  • Forum
  • Documents
  • Polls
  • Quiz
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wireless to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: MAb
  • Date Created: 3 Dec 2014 10:40 AM Date Created
  • Views 1113 views
  • Likes 0 likes
  • Comments 1 comment
  • wifi
  • Processor
  • qoriq
  • freescale
  • 802.11ac
  • freescaledoc
  • wireless
  • standard
  • communication
Related
Recommended

Next-gen WLAN: What you need to know about 802.11ac and why 2.5 Gbps is critically important

MAb
MAb
3 Dec 2014

This article was published first on embedded beat (Freescale blogs) by Eric Dudley, product Marketer at Freeescale

 

WLAN Next Gen blog

 

Wireless data access is everywhere and quickly becoming a staple service in our connected lives, as 3/4G, LTE and WLAN are often our primary communication interfaces. Anyone who has ever exceeded their data plan or who prematurely drained their phone’s battery knows WiFi is the preferred network when it’s available. However, WiFi access is not without its challenges, both from the user’s perspective and the enterprise or service provider’s point of view.

 

Problems around logging in, roaming, performance in congested areas, and security plague users who simply want to download a podcast in the airport, find a nearby restaurant, or watch a video of their nephew on a skateboard. Meanwhile, access control, authentication, and quality of service haunt enterprise and service providers who are forced to accommodate today’s bring-your-own-device users who seek high-speed connectivity, but who may be encroaching on paid customers or private WLANs.

 

Adding to these issues is the new WLAN 802.11ac specification. Instead of sharing a few hundred Mbps of bandwidth among all customers, each user may have that much dedicated bandwidth for themselves! Sounds like a great thing right?  Certainly.  But with all of that new wireless bandwidth, the wired connection from the small access point back to the main network quickly becomes the bottleneck. This link is typically an older copper twisted-pair cable rated to support 1 Gbps.  New 802.11ac WLAN access points can easily drive greater than 1 Gbps speeds and will likely support well over 2 Gbps.  Enter new 2.5 and 5 Gbps Ethernet. This unique, single-twisted pair copper wire technology supports the increased performance that 802.11ac links will require, but without the need to call a contractor to install expensive new cabling.

 

Another related issue of this higher performance 11ac WLAN traffic is that the access points need to get smarter.  Passing all of wireless user data back over the wire to the master controller for decisions about traffic type, quality of service or even access permission will quickly force that appliance to become not only bigger, but much more expensive.

Next-generation 11ac WLAN AP processors will need to deliver 2-4x the performance of earlier access points to solve the traffic jam of a centralized controller making all of the decisions.  This allows the network designer to push the initial use access, filtering and quality checkpoints out to the edge of the network, increasing performance and relieving pressure on the central controller.  Needless to say, Freescale QorIQ processors, with leading market share in enterprise and service provider access points, are again out in front, supporting both 2.5 and 5 Gbps Ethernet over legacy copper cabling.  The QorIQ T1 processor family also gives 2-10x performance over earlier generation products for a lot more intelligence in the WLAN access point.

 

In essence, the next generation of 802.11ac access points will give more dedicated user performance, have fatter 2.5 or 5 Gbps copper pipes, and will make smarter decisions closer to your phone, laptop or tablet.  In the future as you stream your Ultra HD video without a hitch, thank the smart access point and the new high-speed 2.5 and 5 Gbps Ethernet!

 

Eric Dudley is a product marketer for Freescale QorIQ communications processors.

  • Sign in to reply
  • gervasi
    gervasi over 11 years ago

    I've been interested in high-throughput Wi-Fi for a long time.

     

    A few weeks ago I tested throughput on two Gateworks computer boards using 802.11ac cards.  I got three-stream 40MHz channels working.  The 40MHz gives you an easy doubling of throughput at the price of 3dB of link budget.  The multi-stream is trickier.  You have to have a decent channel function with some short and uncorrelated delay spreads between the antennas.  The ac standard supports 80 MHz, but my radio cards didn't support it.  In my Gateworks test I got several hundred Mbps, bridging to computers.

     

    I would love to test a computer board with the QorIQ processor with ac cards.