Wireless
  • Technologies
  • More
Wireless
Blog Wireless Power Charging Device - Powermat 3X
  • Blog
  • Forum
  • Documents
  • Polls
  • Quiz
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wireless to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: sleuz
  • Date Created: 27 Sep 2012 1:28 PM Date Created
  • Views 501 views
  • Likes 0 likes
  • Comments 0 comments
  • charging
  • smartphone
  • wireless_power
  • devices
  • portable
  • Qi Compliant
  • cameras
  • power_system
  • qi_standard
  • mobile
  • media
  • powermat
  • wirelessly
  • independent
  • Easy
  • hand-held
  • wireless_power_consortium
Related
Recommended

Wireless Power Charging Device - Powermat 3X

sleuz
sleuz
27 Sep 2012

Powermat 3x

 

 

 

For your wireless charging needs, the best product on the market, and winner of the TopTenREVIEWS Gold Award, is absolutely the Powermat 3X. This simple, gray mat provides wireless power to a large number of different devices. The variety of devices that this wireless charger can power is impressive, as is its set of features and the customer support that backs it. The Powermat was impressive in every category that we rated these devices on and it consistently outperformed the competition. If you’re looking for a wireless charger for your smartphone or other device, this is the best solution out there.

 

http://www.toptenreviews.com/i/rev/scrn/medium/51646-powermat-3x1.jpg

 

Powermat was founded in 2007 as a result of the huge boom in mobile technology. In their view, the natural progression of mobile technology involves complete wire-free operation, especially for charging. With this idea in mind, they began work on the first Powermat wireless charger. This is the first company to make inductive wireless chargers widely available. This increasingly popular technology has spawned a variety of different products as a result, but none quite match the elegance and efficiency of the Powermat wireless charger.

Powermats use induction technology to charge your mobile devices. This works by transferring electricity from the charger to your phone through magnetic fields. So, when you drop your smartphone or other compatible mobile devices on the wireless charger, charging can begin even without precise, uninhibited contact with a conductive surface.

 

 

The Powermat is compatible with nearly every major smartphone in circulation. They provide cases, skins, sleeves and battery doors for everything from the iPhone to the Blackberry Curve. They even have cases for the Nintendo DS and DSi.

To solve incompatibility with older phones, the manufacturers have added a small device called a “Powercube” to this mat, offering the Powermat 3X with Powercube for a bundled price. This Powercube contains specialized tips that will allow you to use a small cord attached to the Powermat with almost any device. The tips include mini USB, micro USB, an Apple connector and a Sony PSP tip, along with a variety of others. With this wireless charger, no matter what you want to charge, your Powermat can house it all in one convenient product.

 

http://www.toptenreviews.com/i/rev/scrn/medium/51646-powermat-3x3.jpg

 

The maximum number of devices that the Powermat 3X wireless charger can accept at one time is three. Three sections of the mat divide the charging stations into easily visible squares, allowing each device to pull as much energy as it needs to obtain a full charge. The maximum output wattage is 18, which is more than enough to charge multiple smartphones simultaneously.

One of the major features of the Powermat 3X is its internal battery. This device holds a charge of its own, so rather than being stuck in the wall permanently, your Powermat can be charged itself and then taken with you. This added flexibility is reason enough to consider the purchase; this wireless phone charger can be charged and taken with you to give power to your mobile devices wirelessly wherever you go.

 

The Powermat 3X is solid and well-constructed. Better yet, it even feels heavy-duty. We didn’t go as far as actually breaking the wireless charger, but light stress and fall tests proved that this wireless charger is resilient. Its solid construction and compact design make it great for travel, consolidating all of your charging needs into one durable location.

 

 

If you’re looking for the best wireless charger on the market, the Powermat 3X is the device for you. Its immense compatibility (especially when paired with the Powercube) means you will be able to charge almost any device. It comes with a great deal of helpful customer support, including everything from a warranty to a thorough FAQs section. Its travel flexibility, along with a healthy power output and the ability to charge three devices at once, make this the king of wireless phone chargers.

 

 

 

Get more about wireless charging on Wireless-Power-SolutionMore information on www.toptenreviews.com