Wireless
  • Technologies
  • More
Wireless
Forum USB or Ethernet to replace RS232?
  • Blog
  • Forum
  • Documents
  • Polls
  • Quiz
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wireless to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 219 subscribers
  • Views 788 views
  • Users 0 members are here
Related

USB or Ethernet to replace RS232?

M0DCD
M0DCD over 17 years ago

I have had a discussion about this in email, on the subject of replacing RS232 interfaces with either of these two options.

 

My points are that if the item only needs local connectivity (ie download data, setup machine etc) then a generic USB solution such as provided by the FTDI modules is adequate, rather than have to go through having to redesign an existing product. Field service seems to be one application where the technology has run forward (you try and find a laptop with RS232 on it these days). Yes you could use a dingle, but then doesn't Windows keep changing the port number for you?

 

TCP/IP is nice, but if you don't need the machine permanently connected to a network or just have a basic interface, it may be too good a solution. Yes, you can add extra features and a web interface, but would a water level monitor (for instance) that only communicates twice a year need this?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 17 years ago

    We do a fair bit of RS232 because its easy to use and has been around since the electron was discovered imageand we use the FTDI modules. Out in the field we use a Netbook running Linux rather than windows with VMware Worstation (on a laptop running Linux) to run any legacy windows apps. Frankly adding a USB dongle is the best option and if it gets zapped by some surge or other you replace the dongle not the whole shebang. Netbooks running Linux are terrific for field engineering, light small long battery life and don't cost an arm and a leg to replace if they get thumped. A bit off topic I know but RS232 has shifted out of the mainstream so I would suggest dongles and commodity hardware is the way to go.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 17 years ago

    We do a fair bit of RS232 because its easy to use and has been around since the electron was discovered imageand we use the FTDI modules. Out in the field we use a Netbook running Linux rather than windows with VMware Worstation (on a laptop running Linux) to run any legacy windows apps. Frankly adding a USB dongle is the best option and if it gets zapped by some surge or other you replace the dongle not the whole shebang. Netbooks running Linux are terrific for field engineering, light small long battery life and don't cost an arm and a leg to replace if they get thumped. A bit off topic I know but RS232 has shifted out of the mainstream so I would suggest dongles and commodity hardware is the way to go.