Wireless
  • Technologies
  • More
Wireless
Forum mini wireless
  • Blog
  • Forum
  • Documents
  • Polls
  • Quiz
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wireless to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 221 subscribers
  • Views 1585 views
  • Users 0 members are here
Related

mini wireless

R_Phoenix
R_Phoenix over 15 years ago

Whats the smallest way to transmit data?

Max distance would be about 150 feet.

Thanks

  • Sign in to reply
  • Cancel
  • Eavesdropper
    Eavesdropper over 15 years ago

    I'm not sure what you mean by "smallest way."

     

    But, how about non-existent. Go wireless.

     

    E

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • R_Phoenix
    R_Phoenix over 15 years ago in reply to Eavesdropper

    Sorry for not being clear, but yes I want to go wireless - so, how small can I make the transmitter and reciever?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Bengt
    Bengt over 15 years ago in reply to R_Phoenix

    Thats depend on the many you want to spend. There are very small RF transmitters, modules for Bluetooth, Zigbee and WLAN. It is just to many parameters to be able to give suggestions. Data rate, power consumption.....

     

     

    Kontrollera Bluetooth
    AfrikaansAlbanianArabicArmenianAzerbaijaniBasqueBelarusianBulgarianCatalanChinese (Simplified)Chinese (Traditional)CroatianCzechDanishDetect languageDutchEnglishEstonianFilipinoFinnishFrenchGalicianGeorgianGermanGreekHaitian CreoleHebrewHindiHungarianIcelandicIndonesianIrishItalianJapaneseKoreanLatinLatvianLithuanianMacedonianMalayMalteseNorwegianPersianPolishPortugueseRomanianRussianSerbianSlovakSlovenianSpanishSwahiliSwedishThaiTurkishUkrainianUrduVietnameseWelshYiddish⇄AfrikaansAlbanianArabicArmenianAzerbaijaniBasqueBelarusianBulgarianCatalanChinese (Simplified)Chinese (Traditional)CroatianCzechDanishDutchEnglishEstonianFilipinoFinnishFrenchGalicianGeorgianGermanGreekHaitian CreoleHebrewHindiHungarianIcelandicIndonesianIrishItalianJapaneseKoreanLatinLatvianLithuanianMacedonianMalayMalteseNorwegianPersianPolishPortugueseRomanianRussianSerbianSlovakSlovenianSpanishSwahiliSwedishThaiTurkishUkrainianUrduVietnameseWelshYiddish
    Detect language » Swedish
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    One way or both (simplex or duplex ?)

    If, as I'm assuming, your data is going from the "small" unit to a distant base, then I'd probably recomend an OOK transmitter on the 433MHz ISM band. SAW resonators can be had in 3x3mm packages, and a two transistor oscillator + buffer circuit will probably do

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    Alternatively, there are 868MHz transmitter chips in SOT23 or MSOP8 packages, which can be combined with a few 0402 parts and a crystal (5x3mm or smaller)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Myk, (I also read your columns in EWW): 433 MHz is in the centre of the 430 - 440 MHz radio / T.V. amateur band, and the carrier frequency for ATV is 434.250 MHz; we have enough various applications of "low power" status (here, that's 10mW maximum) that interfere with our research efforts as well as each other, so I would really recommend the 868 MHz transmitter solution which suffers far less and affects other users less as well in my professional as well as amateur experience (I was a Space Electronics Engineer especially involved (in the ground segment) with telemetry distribution using a  UHF link series.

    Another common consumer problem arises too from the 433 MHz usage - older car-door-keys that use this range for locking / opening of car doors, I've seen occasions of people "hopping mad" because their "car door won't work" when near an ISM transmit source, which is often not referred to the 10 mW limit but maybe around 100mW or so, 10dBm above what is supposed to be allowed but is not policed effectively in any way most of the time.

    Just my own views and experience - Trevor Gale.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • R_Phoenix
    R_Phoenix over 15 years ago in reply to e14 Contributor

    I found these

    http://www.laipac.com/gps_rf_components.htm

     

    Is there anything smaller?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to R_Phoenix

    Hi R_P,

     

    Well, if you want smaller physical size, then you might look at the Nordic NRF24L01GNRF24L01G+ http://www.sparkfun.com/products/690 , however you'd need to do work to add an aerial etc, like this: http://www.sparkfun.com/products/152. You'll find some cool NRF24L01GNRF24L01G+ options at a cheaper price on eBay too, however they are "bigger". The bigger profile "ready made" boards might help you to learn/ prototype.

     

    Another option along these lines is the Texas Instrument chips: eg. the CC2530, CC2540, etc http://focus.ti.com/analog/docs/rfifcomponentshome.tsp?

     

     

    What mirocontroller are you using? If you're new to wireless and are using Arduino, then you might want to do some hands on research first. The 1MW Xbees (e.g. element14: XB24-AWI-001XB24-AWI-001) would arguably be the easiest place to start. They simplify a lot of the comms management you'll need to do with the cheaper 433Mhz RF options, and there are lots of code libraries and examples available for xbee. Of course, they are "bigger" and they cost more image.

     

    SeeedStudios RFBee is also another interesting option http://bit.ly/gLlztW with its built in Atmega168 AVR. So, as its AVR is combined, this might help you with size.

     

    If 868 or 915Mhz appeal, then the JeeNode might be a good prototyping choice: http://jeelabs.com/products/jeenode.

     

    Cheers,

     

    Paul

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • vittally
    vittally over 15 years ago

    Hi R_Phoenix,

     

    What about a transceiver with a size of 16x32mm like this one: http://uk.farnell.com/adeunis/arf7580aax-un/module-rf-twimo-mp868/dp/1847388 ?

    image

    Cheers,

    Laurent

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Bengt
    Bengt over 15 years ago

    I have found the modules from RFM the best. Reliable and very easy to use.

    AfrikaansAlbanianArabicArmenianAzerbaijaniBasqueBelarusianBulgarianCatalanChinese (Simplified)Chinese (Traditional)CroatianCzechDanishDetect languageDutchEnglishEstonianFilipinoFinnishFrenchGalicianGeorgianGermanGreekHaitian CreoleHebrewHindiHungarianIcelandicIndonesianIrishItalianJapaneseKoreanLatinLatvianLithuanianMacedonianMalayMalteseNorwegianPersianPolishPortugueseRomanianRussianSerbianSlovakSlovenianSpanishSwahiliSwedishThaiTurkishUkrainianUrduVietnameseWelshYiddish⇄AfrikaansAlbanianArabicArmenianAzerbaijaniBasqueBelarusianBulgarianCatalanChinese (Simplified)Chinese (Traditional)CroatianCzechDanishDutchEnglishEstonianFilipinoFinnishFrenchGalicianGeorgianGermanGreekHaitian CreoleHebrewHindiHungarianIcelandicIndonesianIrishItalianJapaneseKoreanLatinLatvianLithuanianMacedonianMalayMalteseNorwegianPersianPolishPortugueseRomanianRussianSerbianSlovakSlovenianSpanishSwahiliSwedishThaiTurkishUkrainianUrduVietnameseWelshYiddish
    Detect language » Swedish
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>