Wireless
  • Technologies
  • More
Wireless
Forum Signal converter 0-20 from 0-50
  • Blog
  • Forum
  • Documents
  • Polls
  • Quiz
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wireless to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 221 subscribers
  • Views 648 views
  • Users 0 members are here
  • conversion
  • communication
Related

Signal converter 0-20 from 0-50

ZeroSizeObject
ZeroSizeObject over 15 years ago
I need to convert a 0-50mA signal to 0-20mA values. I was looking at a API 4300G, but it seems I can not get one at the moment.
 
What are some other options I could try?
 
Zero
  • Sign in to reply
  • Cancel
  • KennyMillar
    KennyMillar over 15 years ago

    Hmmm. The API 4300G is for use in industrial cabinets. Is that what you are after?

    Is this a digital signal, ie: 0 mA  = Logic 0, 100mA = Logic 1, or is it an analogue signal where you have to scale down a constantly variable signal from 0-100 mA down to 0 - 20 mA ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    The first you need convert 0-50mA to voltage, then design a constant current circuit using OPAMP,  so the voltage can cotrol the output current ,  and you need set the ratio equal to 40%.  I have ever used this method.But I don't know if there is a better way.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • lpetacchi
    lpetacchi over 15 years ago

    Do you need isolation or anticipate large common mode voltages between the two loops?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to lpetacchi

    if he need isolation, can Use linear optical coupling