Wireless
  • Technologies
  • More
Wireless
Forum AppInventor2-Android-Arduino-Bluetooth-Previous reading is overwritten
  • Blog
  • Forum
  • Documents
  • Polls
  • Quiz
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wireless to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 1 reply
  • Subscribers 219 subscribers
  • Views 1120 views
  • Users 0 members are here
  • android
  • bluetooth
  • app
  • arduino
Related

AppInventor2-Android-Arduino-Bluetooth-Previous reading is overwritten

e14 Contributor
e14 Contributor over 11 years ago

AppInventor2- How to freeze Display-Value?

 

Previous reading is overwritten!

 

I am working on an Android-Arduino Interface to communicate and send at least 10 different values in both directions.

I am reading with the Android-Phone the Ports of an Arduino Mega2560. On the Serial-Port 1 is a BTM220 Bluetooth-Module.

The Phone sends for reading each Port of the Arduino the characters ‚a‘ for Port A, ‚b‘ for the Port B and so on.

The Output on the Phone-Display is:
PortA= 0bxxxxxxxx,
PortB= 0bxxxxxxxx,
PortC= 0bxxxxxxxx

…….

The Arduino+BTM222 send the Port-Values as strings.

The Problem I have, is that the Phone-Bluetooth reading routine overwrites the screen of the Phone with new values even if I do not ask for any new values (the Phone is not sending any enquiry and the Arduino+BTM222 sends no values). That means that the Arduino does not send any new value, but the Phone-Bluetooth is already reading the next value. The result is that I see for 2 seconds (clock-Delay in the App-Inventor-Routine) the value I have asked for, but 2 seconds later these values are deleted (or overwritten with empty Strings??) while the phone is not asking for any new values from the Arduino
->from the Arduino are no values coming-> the BT sends no values to the phone, but in the phone are the old values deleted/overwritten)

Is there any possibility to “freeze” the first incoming values so that only if the phone sends a new enquiry(Click the Enquiry-Button) the old values will be with the new ones overwritten?

Please help!

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    I have solved the Problem with TinyDB.

    Thanks!

     

    Atron

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer