Wireless
  • Technologies
  • More
Wireless
Forum ZigBee, would this Ad Hoc network idea work?
  • Blog
  • Forum
  • Documents
  • Polls
  • Quiz
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wireless to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 220 subscribers
  • Views 1960 views
  • Users 0 members are here
  • bluetooth
  • network
  • nodes
  • mesh-network
  • wireless
  • zigbee
  • communication
Related

ZigBee, would this Ad Hoc network idea work?

e14 Contributor
e14 Contributor over 11 years ago

 

I’m trying to get a general understanding for how a mesh Ad Hoc network could be created. ZigBee seems as a cheap solution so that’s why I’m going for it. However if you guys have a better suggestion (i.e. Bluetooth) feel free to suggest it.

 

Ok, here goes. My basic idea is this. I have moving objects (large area indoors) and I want to construct a simple warning system. When one device detects another I basically just want to play a tune or make a light flash, nothing more. The approach will probably be using RSSI but that is not important right now. I want this to be cheap and I do not want any kind of fixed infrastructure (disqualifying wifi). The devices would randomly come into contact, do some kind of handshake, talk while they are close and finally move out of range.


Is it even possible to create such a thing with ZigBee? The standard requires a ZigBee Coordinator so I was thinking that one moving object could be this and the rest ZigBee routers. Would this approach even work? Perhaps one could equip a few Raspberry Pi’s with “XBee ZB ZigBee RF Modules” and then take it from there.

 

 

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 11 years ago +1
    How many nodes would be the maximum? t seems you could use any low-cost radio with a small associated CPU for this application as long as collisions can be detected. It probably wouldn't need a big complicated…
Parents
  • gadget.iom
    0 gadget.iom over 11 years ago

    Is there a proximity range you're interested in?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to gadget.iom

     

    I’m trying to create a warning system so the further away one node can detect another, the better. We are talking running speed so guesstimating the reaction time… let’s say at least 5-10 meters/yards. If I can’t get a connection in time it would defeat the purpose of the whole idea.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gadget.iom
    0 gadget.iom over 11 years ago in reply to e14 Contributor

    Have a look at these modules...

    http://www.dx.com/p/433mhz-rf-transmitter-module-receiver-module-link-kit-for-arduino-arm-mcu-wl-green-220194#.ViDtvrzvFHg

     

    You could have one of each in your devices.

    The transmitter sends out a pulse every second for example.

    The receiver can listen for any responses.

     

    You would probably need to disable the local receiver while transmitting, or the device would react to its own transmitter.

    A better approach would be to transmit a code unique to each device, so the receiver can continuously listen, but ignore its own code.

    This could also prove useful in team based games.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • gadget.iom
    0 gadget.iom over 11 years ago in reply to e14 Contributor

    Have a look at these modules...

    http://www.dx.com/p/433mhz-rf-transmitter-module-receiver-module-link-kit-for-arduino-arm-mcu-wl-green-220194#.ViDtvrzvFHg

     

    You could have one of each in your devices.

    The transmitter sends out a pulse every second for example.

    The receiver can listen for any responses.

     

    You would probably need to disable the local receiver while transmitting, or the device would react to its own transmitter.

    A better approach would be to transmit a code unique to each device, so the receiver can continuously listen, but ignore its own code.

    This could also prove useful in team based games.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to gadget.iom

     

    I’m more interested in creating a WPAN. I want to be able create and evaluate some kind of Ad Hoc network providing both a medium access control and the physical layer. Something of the shelf. The modules you are referring to would require me to do all the low layer work. For example when multiple nodes are close, transmitting and receiving uncontrollably, it would all (excuse the language) go to hell.

    My question is more about the architecture of ZigBee. Can you have one node being the ZigBee Coordinator (this part is a must) and all the others being ZigBee Routers?

    From what I see ZigBee end devices can only
    talk to the parent node (either the Coordinator or a Router) meaning that if two ZED’s meet they wouldn’t be able to talk