Wireless
  • Technologies
  • More
Wireless
Forum Propagation of different frequencies
  • Blog
  • Forum
  • Documents
  • Polls
  • Quiz
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wireless to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 1 answer
  • Subscribers 219 subscribers
  • Views 1013 views
  • Users 0 members are here
Related

Propagation of different frequencies

ratsept
ratsept over 16 years ago

Hello everyone,

 

This is my first post here and I really don't know if this is the right place to ask this but...

I am developing a project where we need to track mining equipment in underground mine shafts. The problem is GPS obviously doesn't work underground so our solution is to use small stationary transmitters embedded in the walls of the shafts and with each trackeble piece of equipment carring a receiver we record the time and ID of a transmitter. The transmitters have to be cheap and very low power as we are planning to make them disposable. The receivers are usually mounted on trucks and such and don't need to be very efficient. We considered RFID but that could become very expensive if every piece of equipment would need a several thousand Euro standalone RFID reader. So we went with low powered active beacons and receivers. Well all is well when testing in the office - we get ample range (upto some 100m in open space) and reliable detection but when we take the equipment outdoors in the rain or snow we get problems. We tried 2.4 GHz and it was very cheap and efficient, but we had trouble when the receiver or transmitter were near the ground or a big mass like a truck. Snow and moisture had very little effect on range. Next we tried RFM12B modules at 868 MHz that were unbelievably cheap but also performed well below levels advertised in datasheets. We could get the range but power usage was unacceptable because of low transmission speed and high packet loss. Now we have new modules and are just about to begin testing them but as these are 868 MHz again I have my doubts.

 

I would like to know if anyone has any experience with anything like this and any helpful pointers would be greatly appreciated. Especially any insight into what does and underground environment do to different frequencies and is this even feasible.

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 16 years ago +1
    Hi Tiit I would recommend that you you a lower frequency in your situation. A narrow band VHF module (like 173MHz made by Radiometrix) or a 433MHz one may work better tah the 868s. I woud recommed "Radiometrix…
Parents
  • e14 Contributor
    0 e14 Contributor over 16 years ago

    Hi

    I did two products with radiomodule from Radiocraft RC1140. One hase been used for sport events (indoors/outdoors also under ground), the other product has been used in life jacket. I got good result with two different antennas, PCB and multiloop. I'm using PCB antenna when I have short distance and no snow or water on the antenna. Multiloop I have been used in snow and over sea. The output power has been 9dBm and the frequncy 434MHz. My devices is working both as point to point or point to multipoint. This is an easy configuration in the radiomodule. Please also have a look at company shortlink, they have good modules.

    Best regards

    Torbjörn

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 16 years ago

    Hi

    I did two products with radiomodule from Radiocraft RC1140. One hase been used for sport events (indoors/outdoors also under ground), the other product has been used in life jacket. I got good result with two different antennas, PCB and multiloop. I'm using PCB antenna when I have short distance and no snow or water on the antenna. Multiloop I have been used in snow and over sea. The output power has been 9dBm and the frequncy 434MHz. My devices is working both as point to point or point to multipoint. This is an easy configuration in the radiomodule. Please also have a look at company shortlink, they have good modules.

    Best regards

    Torbjörn