Wireless
  • Technologies
  • More
Wireless
Forum Radio Freq Antennas
  • Blog
  • Forum
  • Documents
  • Polls
  • Quiz
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wireless to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 220 subscribers
  • Views 971 views
  • Users 0 members are here
Related

Radio Freq Antennas

e14 Contributor
e14 Contributor over 15 years ago

I know this sounds archaic, but I have a local public radio station I love listening to, on the AM band.  There are times when there is little static interfearance and times when the static overwhelms the broadcast.  Who can I consult about clearing up AM signal reception by improved antenna or damping interfearance from other sources (? dirty utility line current)??

  • Sign in to reply
  • Cancel
Parents
  • jvdberg@ieee.org
    0 jvdberg@ieee.org over 15 years ago

    Improving reception of medium wave broadcast stations. The reception of medium wave broadcast stations has become worse for several reasons. The receivers that are sold nowadays still have the possibility to tune to the medium wave band. The quality of the AM-part of most receivers is not better than that of the cheapest portable radio. With modern techniques this could be much better. With a communications receiver the reception is much better. However, the filters in most modern communication receivers are too small for high fidelity reception. While the performance of the receivers is decreasing, the interference levels increase as a result of the use of digital circuits, switched mode power supplies, energy saving lamps, digital motor control etcetera. In some areas the interference levels are so high that the reception of medium wave broadcast stations is almost impossible. But to solve your problem, what can you do? Most man made noise is distributed mainly by the mains wiring. Even at a short distance of a building the reception is much better. Using an outdoor antenna will help. Coupling the antenna signal via isolated RF transformers prevent common mode ground signals to enter the receiver. Ferrite rod antennas can be connected to a coaxial cable, using an extra winding of one or two turns. Big antennas are not necessary, the signal strength is high. Unfortunately the noise level is also high. A receiver made before 1970 or an old car radio is sometimes much better than a modern receiver. You could decide to build your own radio or improve an existing radio. High sensitivity is not important. Narrow bandwidth and high dynamic range are. The use of a synchronous detector in stead of a simple diode detector will reduce the unwanted signal output. Signals in the upper sideband and signals in the lower sideband that are not related to the carrier are reduced this way. In some radio receivers the coupling capacitors are too big. The result is that small clicking noise pulses with high amplitude are rectified in the RF and IF amplifiers and temporary change the bias voltages setting of those amplifier stages after each pulse.  This way the small pulses are widened and distortion will occur. Replacing those capacitors by capacitors with a lower value might help. Resulting noise pulses can be clipped or cut out using a noise limiter or noise blanker circuit. As you can see there is a lot to improve. I hope this information will help you to improve the reception of your favourite radio station.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to jvdberg@ieee.org

    jvdberg, your post is greatly appreciated and your knowledge is impressive.  I have been interested in all things electronic all my life, but my background and profession are completely apart from that.  consequently, your post is a bit over my level of understanding.

    so please, if you will, allow a specific question or two that stem from your post:

    [my receiver is a rel new, expensive do everything box with HDMI switching for my TV etc & I'd like 2 see what I can do with RF AM signal interfearance on that device w/o rewiring anything inside that box]

    - do I remove the ferrite bar, connect a coax running 2 a better location and put the ferrite bar on the distant end of the coax?  and, what did u mean by an extra turn (of wire) or two to do the connection?

    - i am purchasing an in-home elect power line noise filter for use on a branch circuit that has hard-wired smoke detectors that talk to each other & a few more plug-in noise filters to go on the power cord ends of several suspect appliances for my home (by suspect, i mean likely a source of line surges since they have motors-compressors;  these from www.X10.com (items XPF-TEL and XPPF-CS-122205-TEL).  do you think this would help my AM RF reception?

    thanks 4 your interest & expert commentary.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to jvdberg@ieee.org

    jvdberg, your post is greatly appreciated and your knowledge is impressive.  I have been interested in all things electronic all my life, but my background and profession are completely apart from that.  consequently, your post is a bit over my level of understanding.

    so please, if you will, allow a specific question or two that stem from your post:

    [my receiver is a rel new, expensive do everything box with HDMI switching for my TV etc & I'd like 2 see what I can do with RF AM signal interfearance on that device w/o rewiring anything inside that box]

    - do I remove the ferrite bar, connect a coax running 2 a better location and put the ferrite bar on the distant end of the coax?  and, what did u mean by an extra turn (of wire) or two to do the connection?

    - i am purchasing an in-home elect power line noise filter for use on a branch circuit that has hard-wired smoke detectors that talk to each other & a few more plug-in noise filters to go on the power cord ends of several suspect appliances for my home (by suspect, i mean likely a source of line surges since they have motors-compressors;  these from www.X10.com (items XPF-TEL and XPPF-CS-122205-TEL).  do you think this would help my AM RF reception?

    thanks 4 your interest & expert commentary.