Wireless
  • Technologies
  • More
Wireless
Forum MIMO
  • Blog
  • Forum
  • Documents
  • Polls
  • Quiz
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wireless to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 218 subscribers
  • Views 713 views
  • Users 0 members are here
Related

MIMO

e14 Contributor
e14 Contributor over 13 years ago

How much better is MIMO capable of significantly increasing wireless data throughput?

  • Sign in to reply
  • Cancel

Top Replies

  • gervasi
    gervasi over 13 years ago +1
    I agree with coder27. There is number of antennas and number of streams. You can have multiple antennas on the TX and/or RX side, and thereby increase the link budget. One way to look at this is if you…
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    I think the speedup is approximately linear, that is, two antennas give about twice the speed

    as one antenna, etc.  But besides increased speed, you also get increased range,

    increased reliability (reduced fading), and increased mobility, and can use multi-path

    algorithms to better handle interference.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • element14jamie
    0 element14jamie over 13 years ago

    Hello Barry,

     

    Welcome to the Community, we hope you are enjoying it. Thank you for your reply coder27. I will move this discussion over to our Wireless Area of teh Community

     

     

     

    Thank you,

     

    Jamie

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gervasi
    0 gervasi over 13 years ago

    I agree with coder27.  There is number of antennas and number of streams.  You can have multiple antennas on the TX and/or RX side, and thereby increase the link budget.  One way to look at this is if you have two antennas xmitting 10mW, you're xmitting 20mW.  If you have two antennas, you have twice the amt of RX energy you're capturing.  You actually get even more improvement than 2x (i.e. 3dB) because MIMO takes advantage of the multipath reflections.  If it's not a rich multipath environment with a delay spread less than the symbol period, you'll just get the 2x improvement from doubling the antennas, which is pretty cool.

     

    If you have good signal strength and a nice multipath channel, you can do dual streams which doubles throughput.  Theoretically you do more than two streams.  I have seen dual stream work on an 802.11(n) card in my own testing.

     

    I've experimented with 802.11(n) 2-stream and seen it work.  Here are the caveats:

    • Two get double the throughput, things have to be just right.  It helps if antennas a different polarizations and/or separated.
    • Sometimes you're better off just using a 40MHz (or 80MHz channel) and getting your extra throughput that way.
    • Most commercial equipment has a poor algorithm to select when it's a good time to use dual-stream.
    • If the data is going over TCP, delays waiting for the TCP ACK to works its way through become a significant impediment.  Doubling underlying data rate doesn't mean twice the user data rate.

     

    Despite all this, you really can do the seeming impossible:  You can double the amt of data you send over a 20MHz channel simply by adding another antenna and doing dual stream.  You're transmitting two separate streams on the same frequency at the same time, which seems like magic.  You can read more about 802.11(n) and 802.11(ac) MIMO here.