Wireless
  • Technologies
  • More
Wireless
Forum RF Amplifier Usage Question
  • Blog
  • Forum
  • Documents
  • Polls
  • Quiz
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wireless to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Answers 1 answer
  • Subscribers 219 subscribers
  • Views 1261 views
  • Users 0 members are here
Related

RF Amplifier Usage Question

hawkeyethehacker
hawkeyethehacker over 12 years ago

Hello All,

 

I am developing an extremely high frequency RF Transmitter solution and I am confused about the workings of RF Amplifiers.

At the moment I am specifically looking at this transmitter and this amplifier.

 

I have two questions:

 

  1. If I were to apply this in a custom PCB (where the transmitter takes Digital input, converting to an RF Signal, taking that output to the amplifier, which in turn puts it through to an antenna), are these the correct parts for the respective jobs?
  2. Is the output of the Transmitter and output of the Amplifier a co-axial type plug? If not, what is the correct type?
  • Sign in to reply
  • Cancel
Parents
  • waelect
    0 waelect over 12 years ago

    Hi Joshua,

     

    I will have to agree with most of the other comments here as well. The 2 devices just from their titles will not work as the Tx chip is 2.4GHz and the amplifier starts at 6GHz well above the 2.4GHz of the transmitter. Definitely a specialized area is PCB design too as there is a lot of stray capacitance's and Inductance's that are involved in this type of design.

     

    There are plenty of specialized module that can be purchases from places, one being mini-circuits and even on element14/Newark http://uk.farnell.com/jsp/search/browse.jsp?N=2031+203582&Ntk=gensearch&Ntt=rf+module&Ntx=mode+matchallpartial

     

    As a radio technician I too am learning as I progress through University to finer details of high frequencies in PCB design. I think there is a certain amount of secrecy in the question ie not divulging the idea but maybe more specifics are needed in what you are trying to accomplish.

     

    As far as the general questions, 2) coax connectors are an option but so are PCB design antenna which are also plausible. As long as you have the correct impedance matching (usually 50ohm ) it should work OK either way.

    The first question is mute point, you will need to use a different amplifier completely to work with the transmitter.

     

    Malcolm

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • waelect
    0 waelect over 12 years ago

    Hi Joshua,

     

    I will have to agree with most of the other comments here as well. The 2 devices just from their titles will not work as the Tx chip is 2.4GHz and the amplifier starts at 6GHz well above the 2.4GHz of the transmitter. Definitely a specialized area is PCB design too as there is a lot of stray capacitance's and Inductance's that are involved in this type of design.

     

    There are plenty of specialized module that can be purchases from places, one being mini-circuits and even on element14/Newark http://uk.farnell.com/jsp/search/browse.jsp?N=2031+203582&Ntk=gensearch&Ntt=rf+module&Ntx=mode+matchallpartial

     

    As a radio technician I too am learning as I progress through University to finer details of high frequencies in PCB design. I think there is a certain amount of secrecy in the question ie not divulging the idea but maybe more specifics are needed in what you are trying to accomplish.

     

    As far as the general questions, 2) coax connectors are an option but so are PCB design antenna which are also plausible. As long as you have the correct impedance matching (usually 50ohm ) it should work OK either way.

    The first question is mute point, you will need to use a different amplifier completely to work with the transmitter.

     

    Malcolm

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • hawkeyethehacker
    0 hawkeyethehacker over 12 years ago in reply to waelect

    OK, apologies for misunderstanding in the first place and I'll take this advice onboard.