Wireless
  • Technologies
  • More
Wireless
Forum Connect Murata SN8200 to WICED SDK
  • Blog
  • Forum
  • Documents
  • Polls
  • Quiz
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wireless to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 219 subscribers
  • Views 542 views
  • Users 0 members are here
  • wireless
  • murata
  • communication
Related

Connect Murata SN8200 to WICED SDK

e14 Contributor
e14 Contributor over 11 years ago

Dear Everyone

I want to know how can I change the C code inside the Murata SN8200 by using WICED SDK or by using any other software. I need that to be able to connect two Murata SN8200 modules together(One as a master and one as a slave). I will receive the data from the UART interface and forward it using wireless to another Murata.

Thanks for your help.

Ahemd

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 11 years ago

    Just a note that SN8200 and SN8200UFL will only be supported up to WICED SDK2.4.1, because WICED SDK 3.0.1 does not support the STM32F103 which is used in SN8200. SN8205 is footprint compatible replacement of SN8200 and uses STM32F205, which is supported in SDK ver 3. Please use SN8205 moving forward for new design.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 11 years ago

    Just a note that SN8200 and SN8200UFL will only be supported up to WICED SDK2.4.1, because WICED SDK 3.0.1 does not support the STM32F103 which is used in SN8200. SN8205 is footprint compatible replacement of SN8200 and uses STM32F205, which is supported in SDK ver 3. Please use SN8205 moving forward for new design.