Wireless
  • Technologies
  • More
Wireless
Forum Want to ask about spectrum distribution of radio waves specifically for LoRa application
  • Blog
  • Forum
  • Documents
  • Polls
  • Quiz
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wireless to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 216 subscribers
  • Views 7158 views
  • Users 0 members are here
  • lora
  • raspberry pi
  • iot
  • wireless_development
  • wireless
  • rf
Related

Want to ask about spectrum distribution of radio waves specifically for LoRa application

embeddedguy
embeddedguy over 3 years ago

Hi Everyone,

I have a Dragino LoRa module HaT which is compatible with RaspberryPi version 3 and older. I wanted to create a LoRa gateway(single channel) for personal use and evaluation how things work.

I saw that the HaT is compatible with frequencies as follows...

868 MHZ/433 MHZ/915 MHZ(Pre-configure in factory)

https://www.dragino.com/products/lora/item/106-lora-gps-hat.html

The region I am living right now(India) does not have 868MhZ as license free band and also not other two remaining frequencies supported by this shield. However here frequencies from 865 to 867MhZ are license free.

These has created confusion to me weather I could use this shield for my application. Some internet discussion also suggest that the module can be configured to 687 MhZ to be used.

Other suggest even that the 868 MhZ can also be used license free as channels are overlapping with 867 MhZ frequency. This has created confusion to me. It would be helpful to ask and get some insight how these frequency division works.?

On internet there are only a few key information but not details about how it distributed.

  • Sign in to reply
  • Cancel

Top Replies

  • charlieo21
    charlieo21 over 3 years ago +3
    It's license free since 2021. The use of low power equipment in the frequency band 865-868 MHz for short range devices_Exemption from License_Rules, 2021 | Department of Telecommunications | Ministry…
  • shabaz
    shabaz over 3 years ago +2
    Hi, If you can legally operate at 867 MHz then the board will work at 867 MHz, even though it says 868 MHz on it. That's because 868 is a loose term that actually includes channels at 867 MHz part of…
  • Gough Lui
    Gough Lui over 3 years ago +2
    Check with your local radio authority. This is very much country-dependent on the local laws and whatever licenses you hold. Just because certain bands are open for use in certain countries does not…
Parents
  • gustavovelascoh
    gustavovelascoh over 3 years ago

    TL:DR;

    The software or firmware in the gateway handles the frequency channels to use with variations per location/Country. For example, there could be a fw version for 868 MHZ where all the band is free or a version for 868_india. As yours is a single-channel gateway, you can work in the 865-867 range.

    More Details:

    As shabaz  mentioned, the designation "868" or "915" includes some Mhz around that central frecuency. These are proposed as license-free band, however some countries already use those bands full or in part. That's why a combination of channels and bandwidths within the band can be used for LoRaWAN, but that will be very specific to the country radio regulations. I have seen gateway Fw versions like 915_AU, 915_SG, 915_CO for Australia, Singapore and Colombia, respectively. This for multichannel gateways, though.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • embeddedguy
    embeddedguy over 3 years ago in reply to gustavovelascoh

    Yes that's precise information you have mentioned.

    So for this module there is a document which mentions how to set a frequence but it does not cover the detail which frequency will work/not work...

    So, I can do two things. First ask Dragino weather frequency in range of 865-867MhZ is possible to set and then if not ask local regulatory body for guidance.

    The document also mentions how to connect to the TTN.

    image

    www.dragino.com/.../LoRa_GPS_HAT_UserManual_v1.0.pdf

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gustavovelascoh
    gustavovelascoh over 3 years ago in reply to embeddedguy

    I guess you can set "freq" and "freq_2" to something between 865400000 and 866800000

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • gustavovelascoh
    gustavovelascoh over 3 years ago in reply to embeddedguy

    I guess you can set "freq" and "freq_2" to something between 865400000 and 866800000