Wireless
  • Technologies
  • More
Wireless
Forum Product suggestion for wrist-wearable audio streaming project
  • Blog
  • Forum
  • Documents
  • Polls
  • Quiz
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wireless to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 217 subscribers
  • Views 1467 views
  • Users 0 members are here
  • bluetooth
  • audio
  • stream
  • Wearable
  • wireless
Related

Product suggestion for wrist-wearable audio streaming project

wlkr.jk
wlkr.jk over 2 years ago

I've been working on a project to live stream audio to a computer from a watch-sized wrist wearable. I'm looking for OTS parts to build a POC. 

Product needs to be worn on the wrist (I'll 3D print a casing with a strap). I need it to be as small as possible.

Functionality:

  • Receive sound from 3 wired in microphones
  • Receive command from customer SW on computer to start receiving audio from microphones
  • Continuously transmit sound via Bluetooth to a computer
  • Receive command to stop receiving audio from microphones
  • Able to be powered via battery

To date, I've evaluated the Adruino Pro Mini, but realized that the sampling rate is only 10kHz, which isn't ideal for high quality audio. 

So, I've recently switched to a Teensy board, which has a sampling rate of 44kHz. 

HW:

  • Microphone module with MAX9814 amplifier
  • TP4056 for battery charging/management
  • LiPo battery (as the project demands, I cannot have it continuously plugged in via USB to operate
  • HM-10 Bluetooth module
  • Simple LEDs for notifying when commands are initiated and complete

Does anyone have any other recommendations for me? A reference article I can reference to make it functional? 

Thanks for your help!

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 2 years ago +2
    I would suggest a Seeed Studio XIAO ESP32C3 (~$5). It has Bluetooth and battery management built-in.... They make an nRF52840 model with built-in mic as well if that is of interest, but it costs about…
  • wlkr.jk
    wlkr.jk over 2 years ago in reply to dougw +1
    Thanks Doug! I'll have a look at that. Great suggestion.
  • dougw
    dougw over 2 years ago in reply to wlkr.jk +1
    It does Wi-Fi as well , which might be easier...here is an example.... https://www.youtube.com/watch?v=qq2FRv0lCPw and another example... https://www.youtube.com/watch?v=a936wNgtcRA
Parents
  • embeddedguy
    embeddedguy over 2 years ago

    Will you use ble audio stack? Or will you only use Arduino ble?

    There are some options here but that depends on your project needs such as you mentioned higher sampling rate etc...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wlkr.jk
    wlkr.jk over 2 years ago in reply to embeddedguy

    I'm actually considering a move to the ESP32 now given built in capabilities. I will say that Arduino is out of the question at this point. 

    JUst trying to determine if the Teensy or the ESP are the way to go. Thoughts? 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • wlkr.jk
    wlkr.jk over 2 years ago in reply to embeddedguy

    I'm actually considering a move to the ESP32 now given built in capabilities. I will say that Arduino is out of the question at this point. 

    JUst trying to determine if the Teensy or the ESP are the way to go. Thoughts?