Wireless
  • Technologies
  • More
Wireless
Forum Omnidirectional RFID UHF antennas with medium (~25mm) range recommendations?
  • Blog
  • Forum
  • Documents
  • Polls
  • Quiz
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wireless to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 17 replies
  • Answers 2 answers
  • Subscribers 215 subscribers
  • Views 4902 views
  • Users 0 members are here
  • antennas
  • rfid
Related

Omnidirectional RFID UHF antennas with medium (~25mm) range recommendations?

penguin
penguin over 2 years ago

Please bear with me as I couldn't even be considered a novice yet. I'm just a coder with an idea that I want to try out using RFID technology.


I want to identify and record data from passive RFID tags that are up to approximately 10 inches (25 cm) away from the device in any direction. There may be a few inches of low density foam between the antenna and the RFID tags. Small size and weight are important factors. Number of simultaneous tag reads... let's say, up to 5 at a time.

Based on my online research, I've come to the conclusion that a UHF reader is the way to go however, it seems like all antennas are either very short (few inches) or very long range. Can anyone recommend some antennas that might be suitable for these requirements?

Thanks in advance.

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 2 years ago +3
    You didn't mention what region you require operation in, but if it's Europe, then this antenna looks ideal and is low-cost: https://www.digikey.co.uk/en/products/detail/kyocera-avx/9000468/21442857 It…
  • shabaz
    shabaz over 2 years ago in reply to shabaz +3 suggested
    Board with the 868 MHz ceramic patch antenna attached. The underside has the U.FL connector, and should have a 0-ohm resistor, but I've not soldered that in yet (because I want to measure the impedance…
  • shabaz
    shabaz over 2 years ago in reply to shabaz +3 suggested
    Measurements! The results are not significantly different from the datasheet, for almost 2/3 of the frequency span. I wouldn't expect it to be identical anyway since there's no guarantee I tested in…
Parents
  • shabaz
    0 shabaz over 2 years ago

    You didn't mention what region you require operation in, but if it's Europe, then this antenna looks ideal and is low-cost:

    https://www.digikey.co.uk/en/products/detail/kyocera-avx/9000468/21442857 

    It is omni-directional, and I suspect (can't guarantee it, you'd need to try it) that it may support the range you're looking at.

    However, you'd need to mount it to a 70 x 70 mm ground plane, which is pretty easy to DIY (you can get the PCB ground plane manufactured for sub-$10, even in single quantity, from many PCB manufacturers in China).

    If you're in North America, then this antenna looks suitable:

    https://www.digikey.co.uk/en/products/detail/kyocera-avx/9000469/21442939

    Again, it requires the 70 x 70 mm ground plane. If you need more info about how to make the ground plane, let me know.

    (And again, no guarantee it will support the range you're looking for, but at the low price it's definitely worth a shot.

    The ground plane will end up looking something like this (the example here is for GPS, not RFID, but it will be almost identical).

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 2 years ago in reply to shabaz

    Measurements!

    The results are not significantly different from the datasheet, for almost 2/3 of the frequency span. I wouldn't expect it to be identical anyway since there's no guarantee I tested in the same environment or the same orientation. I happened to test with the antenna facing vertically upwards.

    This was my first time using the NanoVNA (there are different models, I have the -H4 model) to measure an antenna. Impressive how good it is. Now I understand why people rave about NanoVNAs, it's justified.

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 2 years ago in reply to shabaz

    Measurements!

    The results are not significantly different from the datasheet, for almost 2/3 of the frequency span. I wouldn't expect it to be identical anyway since there's no guarantee I tested in the same environment or the same orientation. I happened to test with the antenna facing vertically upwards.

    This was my first time using the NanoVNA (there are different models, I have the -H4 model) to measure an antenna. Impressive how good it is. Now I understand why people rave about NanoVNAs, it's justified.

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • anniel747
    anniel747 over 2 years ago in reply to shabaz
    This reply was deleted.
    • Cancel
    • Cancel
  • shabaz
    0 shabaz over 2 years ago in reply to anniel747

    It's close, but part of the discrepancy is because the board is for (hopefully) different patch antennas, not just the Kyocera one.

    Since the patches are of different dimensions, it ended up that for this particular antenna, it won't be completely symmetrical (whereas for some smaller Taoglas and Molex GPS antennas that Jan and I tried in some blog posts a few weeks back, those would be symmetrical on this board (and might matter more for GPS, so I figured it may be better to compromise the board for ISM unfortunately). Since not all the patch antennas may be close to 50 ohm, I needed some space for matching.

    Also with hindsight I should have removed some of the solder resist on the ground plane, to make it easier to attach the test cable for the VNA (I had to scratch it off!). Anyway, that can be a future revision maybe.