Wireless
  • Technologies
  • More
Wireless
Documents PRESS RELEASE -Microchip Technology - Releases Tools for Motor Control Designs That Improve Efficiency and Performance While Reducing Development Time
  • Blog
  • Forum
  • Documents
  • Polls
  • Quiz
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wireless to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: rwang
  • Date Created: 10 Dec 2009 4:56 AM Date Created
  • Last Updated Last Updated: 10 Dec 2009 5:12 AM
  • Views 412 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

PRESS RELEASE -Microchip Technology - Releases Tools for Motor Control Designs That Improve Efficiency and Performance While Reducing Development Time

CHANDLER, Ariz., Dec. 7, 2009 [NASDAQ: MCHP] — Microchip Technology Inc., a leading provider of microcontroller and analog semiconductors, today announced two new low-cost development systems, one for the control of high-voltage motors and another for stepper motors. Along with related applications notes and free source-code software, these development tools enable rapid designs using dsPICRegistered digital signal controllers (DSCs).

 

image

High-res Photos Available Through Flickr or Editorial Contact (feel free to publish):

 

http://www.microchip.com/get/12JT

The new

dsPICDEMTm MCHV Development System

is the industry’s only development tool for the rapid evaluation and design of a wide variety of high-voltage, closed-loop motor control applications using AC Induction Motors (ACIMs), Brushless DC (BLDC) motors or Permanent Magnet Synchronous Motors (PMSMs). The board includes in-circuit debugging circuitry, eliminating the need for a separate debugger for development with Microchip’s dsPIC33 Motor Control DSC families. Additionally, this tool combines a proven motor-control system and Power Factor Correction (PFC) for regulatory requirements.

Watch a video demonstration of the dsPICDEM MCHV at:

http://www.microchip.com/get/PCJT

The new dsPICDEM MCSM Development Board

is the industry’s most cost-effective tool for creating unipolar and bipolar stepper motor applications. This board enables the rapid development of both open-loop and current-closed-loop microstepping routines using Microchip’s dsPIC33 Motor Control families. This development tool also provides engineers with a control GUI, which allows them to focus on integrating the other application features and fine-tuning the motor’s operation.

“These development tools jumpstart our customers’ advanced high-voltage motor control and stepper motor control designs, and brings the benefits of high-efficiency control to their products quickly,” said Sumit Mitra, vice president of Microchip’s High Performance Microcontroller Division. “Both development boards feature the flexible dsPIC33F “MC” DSC families, which integrate leading-edge motor control features. Together, this offers our customers a winning combination of price, features and reduced time to market for their motor control applications.”

 

Software Tools and Libraries

 

Five royalty- and license-free software application notes with source code are being released for development, five with the dsPICDEM MCHV and one with the dsPICDEM MCSM. Designers can utilize Microchip’s proven, optimized and efficient code to produce reliable results, while reducing software creation and debug time:

•

AN957

Sensored BLDC Motor Control Using dsPIC30F2010

•

AN984

An Introduction to AC Induction Motor Control Using the dsPIC30F/dsPIC33F DSCs

•

AN1078

FOC Sensorless PMSM with SMO Estimator, Field Weakening and Dual Shunts

•

AN1160

Sensorless BLDC Control with Back-EMF Filtering Using a Majority Function

•

AN1299

FOC Sensorless PMSM with SMO Estimator, Field Weakening and Single-Shunt

•

AN1307

Stepper Motor Control with dsPICRegistered DSCs

Microchip’s free Field Oriented Control (FOC) software libraries enable the development of green motor-based systems. By using these libraries, the engineer can run motors at their peak efficiency and generate the maximum torque using the minimum amount of energy.

Microchip’s stepper motor control library enables the development of high-speed stepper motor control applications with variable micro-stepping down to 1/64 of a step. By using closed-loop current control, stepper motors can be run several times faster than their rated speeds with high torque and very-low-noise operation.

Included with Microchip’s free

MPLABRegistered IDE

integrated development environment is an application called the Data Monitoring and Control Interface (DMCI). Using this GUI with a USB cable for communications to the target board via the included Real Time Data Monitoring (RTDM) protocol promotes rapid parameter tuning for different motors. Unlike Microchip, other competitor systems require that the motor be stopped, the source code modified, recompiled, downloaded and the DSC or MCU reprogrammed to see the effect of a control parameter change.

 

Pricing and Availability

 

Both tools are available today for purchase from

microchipDIRECT.com or any authorized worldwide distributor. The dsPICDEM MCHV Development System (part # DM330023.DM330023.) is $650. The dsPICDEM MCSM Development Board (part # DM330022.DM330022.) is $129.99, and is also available as the dsPICDEMTm MCSM Development Kit (part # DV330021, $269.99), which includes a stepper motor and 24-volt power supply. For a complete overview of Microchip’s dsPIC DSC motor control solutions, please visit http://www.microchip.com/get/SVSE

.

About Microchip Technology

 

Microchip Technology Inc. (NASDAQ: MCHP) is a leading provider of microcontroller and analog semiconductors, providing low-risk product development, lower total system cost and faster time to market for thousands of diverse customer applications worldwide. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at

http://www.microchip.com/get/QJB6

.

Note: The Microchip name and logo, dsPIC, and MPLAB are registered trademarks of Microchip Technology Inc. in the USA and other countries. dsPICDEM is a trademark of Microchip Technology Inc. All other trademarks mentioned herein are the property of their respective companies.

 

High-res Photos Available Through Flickr or Editorial Contact (feel free to publish):

http://www.microchip.com/get/12JT

 

Video Available Through YouTube or Editorial Contact (feel free to post):

http://www.microchip.com/get/PCJT

 

Tags / Keywords: Motor Control, High Voltage Motor, Stepper Motor, Sensorless, Closed Loop, FOC, ACIM, BLDC, PMSM, Tools

RSS Feed for Microchip Product News:

http://www.microchip.com/get/7H8D

  • pt:events
  • tc:industry
  • sp:microchip
  • at:press_release
  • Share
  • History