Wireless
  • Technologies
  • More
Wireless
Documents PRESS RELEASE - Altera - Ships Stratix IV E FPGA Development Kit Featuring a 530K Logic Element FPGA
  • Blog
  • Forum
  • Documents
  • Polls
  • Quiz
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wireless to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: rwang
  • Date Created: 16 Dec 2009 8:24 AM Date Created
  • Last Updated Last Updated: 7 Oct 2021 1:58 AM
  • Views 1082 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

PRESS RELEASE - Altera - Ships Stratix IV E FPGA Development Kit Featuring a 530K Logic Element FPGA

Develop and Test DDR3 DIMM Memory Subsystems with Stratix IV E FPGA Development Kit

 

San Jose, Calif., December 7, 2009—Altera Corporation (NASDAQ: ALTR) today announced the availability of its latest development kit targeting StratixRegistered IV FPGAs. The Stratix IV E FPGA Development Kit features the industry's highest density, highest performance FPGA available. The kit provides users with a comprehensive design environment that includes the hardware and software needed to immediately begin prototyping their high-density designs.

 

The Stratix IV E FPGA Development Kit is based on a high-performance, high-density Stratix IV EP4SE530 FPGA. The FPGA features 530K logic elements (LEs) and provides on average 25 percent higher performance than currently available competitive FPGAs. The performance and density advantage offered by the Stratix IV EP4SE530 FPGA enables customers using the Stratix IV E FPGA Development Kit to fit their large designs into a single device and achieve fast timing closure.

 

The Stratix IV E FPGA Development Kit is the first kit available to feature an FPGA interfacing with a 533-MHz DDR3 DIMM. Using this kit, customers can develop and test memory subsystems consisting of DDR3 DIMMs, QDR II+, and RLDRAM II memory interfaces.

 

The Stratix IV EP4SE530 FPGA is pin compatible with Stratix III FPGAs. This pin compatibility allows customers to seamlessly migrate their Stratix III FPGA design to a higher density Stratix IV E FPGA. Customers can also seamlessly convert their final Stratix IV E FPGA design to Altera's low-cost HardCopyRegistered IV E ASIC. Upon silicon availability in 2010, customers will also be able to migrate their Stratix IV E FPGA design to a higher density EP4SE820 device, which Altera previously announced in September 2009.

 

The Stratix IV E FPGA Development Kit includes:

 

  • Development board featuring a Stratix IV E EP4SE530 FPGA
  • Board test system with design examples
  • 2-GB DDR3 SDRAM DIMM with a 72-bit data bus
  • 72-Mb QDR II+ SRAM device with a 18-bit data bus
  • 576-Mb RLDRAM  II CIO device with a 36-bit data bus
  • CD-ROM containing design examples
  • NiosRegistered II Design Suite license
  • QuartusRegistered II Design Software, Development Kit Edition (DKE)

 

 

Pricing and Availability

 

The AlteraRegistered Stratix IV E FPGA Development Kit is available today and is priced at $9,995. To learn more about the development kit, or to order, visit www.altera.com/products/devkits/altera/kit-stratix-iv-e.html.

 

About Altera

 

Altera programmable solutions enable system and semiconductor companies to rapidly and cost-effectively innovate, differentiate and win in their markets. Find out more about Altera's FPGA, CPLD and ASIC devices at www.altera.com. Follow Altera via Facebook, RSS and Twitter.

Altera, the Altera logo, and all other words that are identified as trademarks are, unless noted otherwise, Registered, U.S. Patent and Trademark Office, and the trademarks of Altera Corporation in the U.S. and other countries. All other product or service names are the property of their respective holders.

  • pt:embedded
  • pt:dev_kit
  • sp:altera
  • tc:fpga
  • at:press_release
  • Share
  • History