Wireless
  • Technologies
  • More
Wireless
Documents Why you should use Ultra low ESR Super Capacitors in GSM/GPRS applications.
  • Blog
  • Forum
  • Documents
  • Polls
  • Quiz
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wireless to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: Andy_Brook
  • Date Created: 29 Oct 2010 3:38 PM Date Created
  • Last Updated Last Updated: 7 Oct 2021 7:24 AM
  • Views 1465 views
  • Likes 0 likes
  • Comments 1 comment
Related
Recommended

Why you should use Ultra low ESR Super Capacitors in GSM/GPRS applications.

http://www.icd-sales.com/images/product-pics/image-sc.jpg

Why should you use Ultra low ESR Super Capacitors in GSM/GPRS applications?
 
GSM Protocol Requires 2A Pulse for 0.6msec Every 4.2msec
GSM / GPRS modules are implemented mostly in M2M applications. These GSM/GPRS modules use either Lithium Ion rechargeable battery’s or Lithium Thionyl Chloride Battery non-rechargeable - primary. For both type of batteries it is recommend to use CLG04P050L28 or CLG03P120L28 both stocked by Farnell.
 
Case of Lithium Ion battery:
It is recommended to use a non Aqueous Ultra Low ESR Super Capacitor with lower or equal ESR to the internal resistance of the Lithium Ion Battery (~ 150 mΩ).
During the short GSM pick pulse of 2A, the Lithium Ion will deliver a maximum of 1A only.
This reduction will prevent serious "Voltage Recovery" effect (after high current pulse, battery voltage does not achieve it's previous value).
Adding these Super Capacitors will aid preventing the battery to enter "Voltage Recovery". Without a Super Cap the battery alone needs to provide 2A. This high current causes early discharge of the battery and prevents it getting closer to its shutdown threshold.
Between the GSM pulses during 4.2msec the battery can smoothly charge the Super Cap.
 
Conclusion – A low ESR Super Capacitor can contribute to lengthen the time between battery shutdowns. Adding Super Capacitors to GSM design is essential for smooth and longer operation.
 
Case of Lithium Thionyl Chloride Battery:
In cases where the primary battery alone is un able to provide GSM / GPRS 2A pulse. The Super Capacitor with its high capacitance and low ESR enables the required high current 2A short burst. As in the case LiON  example between the 0.6msec GSM pulses, during 4.2msec the battery can smoothly charge the Super Capacitor.
 
Conclusion – A Super Capacitor is mandatory for operation and prevent battery shutdowns.
 
 
To view the range of stocked Cellergy supercaps please click here.
  • clg03p120l28
  • edlc
  • electric_double_layer_capacitor
  • clg04p050l28
  • cellergy
  • chloride
  • gsm_protocol
  • evercap
  • dlc
  • lithium
  • avx
  • double_layer_capacitors
  • tantalum
  • panasonic
  • gsm
  • supercap
  • super_cap
  • thionyl
  • gprs
  • electrolytic
  • ever_cap
  • goldcap
  • bestcap
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply
  • e14 Contributor
    e14 Contributor over 14 years ago

    Thanks for your post above, I am having difficultly with a board which has an Telit module gc864, it keeps intermintently dropping using a single Lithium Thionyl Chloride saft battery lsh20. It seems it cannot provide the 2A peeks. I have an LT1308ACS8#PBF.LT1308ACS8#PBF. buck boost to increase the voltage from 3.6 to about 4 volts and have tried the caps after the buck boost and before the gsm module but the problem persists. I am wondering if you have any reference designs using a Lithium Thionyl Chloride saft battery which you could share.

    Thanks and Regards Mark