Wireless
  • Technologies
  • More
Wireless
Documents USB2SER: USB to Serial Bridge Ready Play Solution~
  • Blog
  • Forum
  • Documents
  • Polls
  • Quiz
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wireless to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: squadMCU
  • Date Created: 14 Jun 2011 5:08 PM Date Created
  • Last Updated Last Updated: 7 Oct 2021 10:29 AM
  • Views 1317 views
  • Likes 0 likes
  • Comments 9 comments
Related
Recommended

USB2SER: USB to Serial Bridge Ready Play Solution~

USB2SER is a USB to UART bridge controller on 5x5mm lead free QFN24. It is a simple low cost solution that enables USB for an embedded system with a UART port, which reduces external components count. It supports USB 2.0 full-speed and TTL RS232 or RS485 UART with options for hardware flow control, software flow control (Xon-Xoff), even or odd parity and stop bits configuration. The USB2SER is fully compliant with the USB 2.0 specification, and it can act as a CDC standard device which eliminates the need for custom drivers for operation when flow-control is not needed (only an INF file is required).

 

http://cache.freescale.com/files/graphic/block_diagram/USB2SER_BDTN.jpg

 

 

Features
Single chip USB to UART Data Transfer (RS232 or RS485)
Certified Full USB 2.0 support - full speed
UART with programmable custom baud rates from 300bps to 115200bps and hardware flow control (RTC / CTS) or Software Xon/Xoff flow control
RESUME signal to request a remote wake-up and SUSPEND output to indicate that the device is in Suspended Mode
Supports 2MHz, 4MHz, 6MHz, 8MHz, 12MHz and 16MHz external crystals with automatic crystal frequency detection
Configurable USB VID, PID and Device Description strings in internal Flash
Configurable Password to protect device from additional parameters modifications
USB2SER comes in a compact 5x5mm Pb free RoHS compliant QFN24
USB2SER can act as a CDC standard device which eliminates the need for custom drivers for operation when flow-control is not needed (only an INF file is required)

Features

- Single chip USB to UART Data Transfer (RS232 or RS485)

- Certified Full USB 2.0 support - full speed

- UART with programmable custom baud rates from 300bps to 115200bps and hardware flow control (RTC / CTS) or Software Xon/Xoff flow control

- RESUME signal to request a remote wake-up and SUSPEND output to indicate that the device is in Suspended Mode

- Supports 2MHz, 4MHz, 6MHz, 8MHz, 12MHz and 16MHz external crystals with automatic crystal frequency detection

- Configurable USB VID, PID and Device Description strings in internal Flash

- Configurable Password to protect device from additional parameters modifications

- USB2SER comes in a compact 5x5mm Pb free RoHS compliant QFN24

- USB2SER can act as a CDC standard device which eliminates the need for custom drivers for operation when flow-control is not needed (only an INF file is required)

 

 

 

http://www.freescale.com/USB2SER

  • freescaledocs
  • sp:analog
  • devices
  • in:communications
  • cdc
  • usb
  • sp:freescale
  • rs485
  • uart
  • rs232
  • serial
  • semiconductor
  • communication
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago
    hey there... sorry for the late response ! Its been a crazy couple of weeks !
     
    When you try to configure the port in a not supported way (anyone), the device responds the request with a Stall, which means that the COM port can’t be opened with that configuration. Supported configurations are from 300 bps to 115200, even, odd or no parity and 1 or 2 stop bits, if customer tries anything outside this in a PC they will get an error indicating that the serial port couldn’t be opened with the desired configuration, if they do this on an embedded system (i.e. running on MQX or Linux), it depends on what the system does when receiving a stall but the port won’t be open.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • bbolo1
    bbolo1 over 14 years ago in reply to e14 Contributor

    Thank you! This is a very good explanation and it is good that the chip provides a mechanism (by stalling the USB pipe) to avoid connection parameters that might be out of the range of supported ones.

    Is there any other package option besides the QFN?

    Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • bbolo1
    bbolo1 over 14 years ago in reply to e14 Contributor

    Thank you! This is a very good explanation and it is good that the chip provides a mechanism (by stalling the USB pipe) to avoid connection parameters that might be out of the range of supported ones.

    Is there any other package option besides the QFN?

    Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • squadMCU
    squadMCU over 14 years ago in reply to bbolo1

    hello bbolo1:

    We think they have only QFN 24 EP 5*5*1.0P0.65

    Check the parametric data on Freescale site:

    http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=USB2SER&nodeId=0143594058&tab=Buy_Parametric_Tab&fromSearch=false

     

    Hope it helps!