Wireless
  • Technologies
  • More
Wireless
Documents ENOCEAN - ESK 300 - KIT, ENERGY HARVEST, W/LESS, 868MHZ
  • Blog
  • Forum
  • Documents
  • Polls
  • Quiz
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wireless to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: RenfordNel
  • Date Created: 3 Jun 2012 7:15 PM Date Created
  • Last Updated Last Updated: 3 Jun 2012 7:20 PM
  • Views 1122 views
  • Likes 2 likes
  • Comments 2 comments
Related
Recommended

ENOCEAN - ESK 300 - KIT, ENERGY HARVEST, W/LESS, 868MHZ

ENOCEAN - ESK 300ESK 300 - KIT, ENERGY HARVEST, W/LESS, 868MHZ | Buy Now!Buy Now!

 

image

 

Product Introduction

 

The  EnOcean Starter Kit has been designed to demonstrate EnOcean’s energy harvesting and ultra low power radio technology.  The ESK 300 comes with two electro-mechanical push button generators for switches and a solar powered temperature sensor. Radio telegrams sent by the selfpowered sensors are received via USB dongle and visualized via DolphinView Basic PC software.

 

ESK 300(C) Content

 

User Manual

USB 300(C): USB Stick Gateway

PTM 200(C): Self powered push button switch

Rocker: Rocker push button switch

STM 330(C): Self-powered temperature sensor

ECO 200:      Push button energy generator

PTM 330(C): Push button radio module

Housing example from SEMD

Housing example from BSC GmbH

 

PTM 200 – Push-Button Switch for Building Automation

 

The push-button radio transmitter module  enables the implementation of wireless remote controls without batteries. Key applications are wall-mounted flat rocker switches with 1 or  2 rockers, as well as handheld remote controls with up to 4 single push-buttons.

 

  • Radio telegrams will be received via USB 300 and shown by DolphinView Basic
  • Press rocker to send switch telegram -> PTM 200 will be shown in node list
  • Select node and press “Set Profile” button to interpret Equipment Profile
  • Press rocker on I-side (marking on PTM 200) to send “switch on telegram”
  • Press rocker on O-side (marking on PTM 200) to send “switch off telegram”
  • Release rocker to send switch telegram “Energy Bow: release”

 

ECO 200 & PTM 330 – Push Button Generator & Radio Module

 

The ECO 200 is an energy converter for linear motion. It can be used to power the PTM 330 radio module. The energy output at every actuation is sufficient to transmit 3 subtelegrams with a free field range of 300m. Possible applications are miniaturized switches and sensors in building technology and industrial automation.

 

  • Radio telegrams will be received via USB 300 and shown by DolphinView Basic
  • Press spring to send telegram -> PTM 330 will be shown in the node list
  • Select node and press “Set Profile” button to interpret Equipment Profile
  • Press spring to send telegram “Energy Bow: pressed”
  • Pull spring to send telegram “Energy Bow: release”

 

STM 330 – Self-powered Temperature Sensor

 

The STM330 is a solar powered module that is optimised for wireless, maintenance-free temperature sensors and room operating panels. It can be extended with a plug’n play humidity sensor.

 

Radio telegrams will be received via USB 300 and shown by DolphinView Basic

Turn the STM 300 with solar cell faced up to get light, indoor light will be sufficient Configure

 

  • DolphinView Basic with EnOcean Equipment Profile with following values and press “Set Profile” button:
    • RORG: 0x0A5 4BS Telegram
    • FUNC: 0x02 Temperature Sensor
    • TYPE:  0x05 Temperature Sensor Range 0°C to +40°C
  • Press the STM 330 button to send sensor telegram
  • The STM 330 sends temperature values every ~1.000s (during darkness for ~100h)

 

Push Button Switch

 

Depending on your locality the ESK 300 will be delivered with housing examples for PTM 330 and the ECO 200. This demonstrates how EnOcean’s energy harvesting and ultra low power radio technology can be implemented within various environments.

 

Switch frame from the company SEMD

 

  • Clip ECO 200 into SEMD plastic frame
  • Clip PTM 330 on top of ECO 200
  • Push tongue to send telegrams

 

Switch housing from company BSC GmbH

 

  • Clip PTM 330 and antenna into upper part
  • Clip ECO 200 with spring inside the gap of the arm into bottom part
  • Put four spacers into the corner of ECO 200 and close housing with screws
  • Push arm to send a telegram

 

 

Man Part No.Description
ESK300ESK300 KIT, ENERGY HARVEST, W/LESS, 868MHZ
ESK300CESK300C KIT, ENERGY HARVEST, W/LESS, 315MHZ 
  • 300
  • esk
  • 2088254
  • enocean
  • 89t3687
  • esk300c
  • 868mhz
  • w/less
  • kit
  • energy
  • 2088255
  • harvest
  • 89t3686
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply
Parents
  • DAB
    DAB over 14 years ago

    It would be interesting to compare these kits with the TI energy harvesting kit.  Both are solar powered and include a temperature sensor, so you could run them in a side by side test to see how the different approaches work.  Plus they area both available for about the same cost, so a good one to one objective test would be useful for people to decide which would better fit their application.

     

    Another good road test candidate.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 14 years ago

    It would be interesting to compare these kits with the TI energy harvesting kit.  Both are solar powered and include a temperature sensor, so you could run them in a side by side test to see how the different approaches work.  Plus they area both available for about the same cost, so a good one to one objective test would be useful for people to decide which would better fit their application.

     

    Another good road test candidate.

     

    DAB