Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Repair Challenge: XBOX ONE S! (Beep on then beep off)
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 57 replies
  • Answers 7 answers
  • Subscribers 316 subscribers
  • Views 37703 views
  • Users 0 members are here
  • xbox
  • helpme
  • repair
  • xbox one s
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Repair Challenge: XBOX ONE S! (Beep on then beep off)

lilithelotor
lilithelotor over 7 years ago

CLARIFICATION

YES, BEFORE STARTING WORK ON THIS OF COURSE I GOOGLED AND WATCHED SEVERAL VIDEOS (MOSTLY USELESS) AND READ RESOURCES ON COMMON XBOX ONE AND ONE S PROBLEMS.

 

  1. I tried the HDD in a PC, and it does show up as several NTFS partitions with files that all look fine.
  2. Blu Ray drive at least powers up and can insert and eject a disc.
  3. Tried the "cold mode hairdrier" trick to spin the fan manually. It's not the fan. The fan works.

All other components of the board seem to work. Just the system started up with a startup sound, and shut down with a shut down sound immediately after. Likely a protection being triggered.

 

Help meee!

 

Trying to figure out this XBOX One S issue: https://www.ifixit.com/Answers/View/523582/PSU+11... Any ideas?

 

It makes the start and then stop sound. Southbridge gets voltage. All 12V test points get voltage. Power rails to CPU suspiciously low resistance. Details in iFixit link.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image


I have an XBOX ONE S that I bought as “for parts” on eBay and the owner says it was kept in a clean house, etc. It is indeed clean inside. No signs of water damage.

The PSU is also fine. The APU had a TON of thermal grease all over the surface mount capacitors. I didn’t remove that yet but I did re-apply some arctic silver and I used a more reasonable amount.

The symptoms I see:

Console when plugged in does a few quick pulses to the APU fan. Is it trying to init?

Console when eject is pressed makes the eject sound, then the shutdown sound immediately after.

Console when power is pressed makes startup beep and then shutdown beep immediately after.

I don’t know what kind of issue I’m getting yet. Is there a JTAG interface or some way to do further diagnosis on this thing?

11.94V sounds perfectly fine for a 12V rail. Should I simpy try plugging a PC power supply into the motherboard to see if it will boot?

Any links or info on diagnosis would be appreciated.

Thanks in advance!


later

Aha! In the image you can see the CPU filter capacitor is registering just 1 ohm! The others are pretty low too but I bet if I remove that one it’ll at least boot. I have a server motherboard with a broken socket that I can steal capacitors from. Might replace the whole row if necessary.

image


later still

Looks like I was wrong. That capacitor I removed still offers up almost exactly the uf value on the tin. So that was another dead end. Hmm... One weird thing, all of the test points register 60Hz but not 110V. So thankfully the PSU isn't pushing wall socket voltage through. But that frequency is weird. My multimeter needs a charge though so I'll measure that again after it has.

The entire power area for the APU offers almost no resistance to the ground plane which is worrying. Again, need to charge that multimeter and re-check.


later again

Power on with no heatsink, the processor doesn't even warm to the touch. CPU, GPU, and other test points around the board pulse to 1-2V and then turn off fast.

Can't help but think it's related to the very low impedance between ground and positive on the V rails for the CPU/GPU. Is that normal?

USB port is charging the multimeter image

So that 5V rail from the southbridge is working.

Lots of 12V test points are consistently 12V (11.94V)


So...

Does any one have a diagram of the test points around the motherboard? What voltages / values should I be seeing? What are some likely culprits?

Thanks in advance! You're all wonderful!

 

This is the original XBOX One. Similar, but not exactly what I need. I can still maybe work from it.

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • Gough Lui
    Gough Lui over 7 years ago in reply to lilithelotor +5 suggested
    Sorry - I've been quite busy and am at work ... supposing you didn't lift any traces or warp the board significantly, you might well be fine. However, that's not to say that the VRM didn't fail for other…
  • lilithelotor
    lilithelotor over 7 years ago in reply to Gough Lui +4 suggested
    You are so wonderful and I can't thank you enough. I will work patiently from now on and I have learned a lot from this process. It is actually the first time I have ever used my hot air rework station…
  • Gough Lui
    Gough Lui over 7 years ago +3 suggested
    Most of the time, VRM issues are blown MOSFETs which have become shorted - your low resistance measurement is suggestive that the MOSFET on that phase may have gone shorted. Short burst of voltage and…
Parents
  • changedsoul
    0 changedsoul over 6 years ago

    I just recently purchased an XBox One S off ebay that had water damage. I was attempting to repair it when much to my surprise, someone had already had a go at it and butchered it up a bit. Watching some videos on youtube i came to the conclusion having a power supply that has current limit ability is invaluable. It makes it very nice to track down shorts and fix them.

    My issue however is a bit worse than yours. I get no power on/off beeps. Checking the voltages, I have 12v, 5v, 3.3v(one of them), 1.8v all present. The board was shorted at the connector where the front panel connects (power, eject, etc) go. It was so badly damaged that I cannot tell what voltages are supposed to be present there. I was "hoping" this post is still somewhat active and someone can assist in these measurements?

    We may very well have a similar issue, but until I can repair what has been trashed, I dont know what is causing my issue.

    image

    If someone would be super kind, and if possible, could someone tell me what voltages should be present on that connector at the bottom middle of the board, on Pin 8, and 7? This is where my board short was and I had to dig out the rot. Now I am left is a mess and need to connect the connectors to what ever power they were getting so I can see what else may be wrong. Pin 8 looks like it may be ground, and Pin 7 looks like it may be coming from that right cap (which I think is 5v),  but before I go and repair it, I would be so grateful if someone could verify the values for me?

    If I can get this working, I will post the solution, and just maybe it will solve the OP issue. I really hope its not the APU

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • changedsoul
    0 changedsoul over 6 years ago

    I just recently purchased an XBox One S off ebay that had water damage. I was attempting to repair it when much to my surprise, someone had already had a go at it and butchered it up a bit. Watching some videos on youtube i came to the conclusion having a power supply that has current limit ability is invaluable. It makes it very nice to track down shorts and fix them.

    My issue however is a bit worse than yours. I get no power on/off beeps. Checking the voltages, I have 12v, 5v, 3.3v(one of them), 1.8v all present. The board was shorted at the connector where the front panel connects (power, eject, etc) go. It was so badly damaged that I cannot tell what voltages are supposed to be present there. I was "hoping" this post is still somewhat active and someone can assist in these measurements?

    We may very well have a similar issue, but until I can repair what has been trashed, I dont know what is causing my issue.

    image

    If someone would be super kind, and if possible, could someone tell me what voltages should be present on that connector at the bottom middle of the board, on Pin 8, and 7? This is where my board short was and I had to dig out the rot. Now I am left is a mess and need to connect the connectors to what ever power they were getting so I can see what else may be wrong. Pin 8 looks like it may be ground, and Pin 7 looks like it may be coming from that right cap (which I think is 5v),  but before I go and repair it, I would be so grateful if someone could verify the values for me?

    If I can get this working, I will post the solution, and just maybe it will solve the OP issue. I really hope its not the APU

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • blockaboots
    0 blockaboots over 6 years ago in reply to changedsoul

    I have a similar issue with my Xbox One S, basically the fault was the mosfet on phase line 3, i was getting a reading of only 0.357v each way with the Multi-meter, when in theory the reading should be 0.648v one way and then 1.917v the other. After i replaced the suspect mosfet i tested with the MM again but i was getting the exact same reading (0.357v). Any ideas why this might be?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • lilithelotor
    0 lilithelotor over 6 years ago in reply to blockaboots

    My only thoughts would be a short elsewhere on the board. I know mine looks like it had minor water damage. Maybe it had been shorted somewhere along the way.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • blockaboots
    0 blockaboots over 6 years ago in reply to lilithelotor

    I tried testing the resistors around the mosfet chip on the other 2 phase lines (which had correct readings for the mosfet) to get an idea of what the resistor readings should be and then i tested the resistors on the bad mosfet phase line and they game me the same results as those on the 2 good phase lines, so i dont think its the resistors that are bad. I also doubt its the coil on each of the phase lines (big black box type thing) as essentially there just coils of wire. Im not sure what else to check, if it is a short else where it has to be a component before the mosfet i guess

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • lilithelotor
    0 lilithelotor over 5 years ago in reply to blockaboots

    Yeah this is a super hard one. I put it down a long time ago. Maybe I should fiddle with it again. I have new MSOFET chips but I may have done other damage to my board by messing around and without schematics or an oscilloscope I am really flying blind.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mysticalbacon679
    0 mysticalbacon679 over 5 years ago in reply to lilithelotor

    Hey im having the same issue but mine had a orange soda spilled on it. The edges where the copper is has dark brown spots on it. Same noises and fan situation as yours, even changed power supplies and still the same thing.  What do you think about that?